On AD9910 EVAL board with crystal mode (25MHz), I config N value in CFR3 for sysClk. Expect to output a DDS sine wave of 50MHz.
CFR1 = 0x00402002
CFR2 = 0x00400820
CFR3 = 0x193F4528 <--- N will be configured from 20, 24, 28, 32, 36, to 40.
FTW in Profile register will be set according to sysClk.
Question: I expected the output freq of 50MHz, but it was not. See below yellow mark (55MHz). Some are over 55MHz, some under 55MHz.
Is there something wrong with my config ? or wrong programming ?