Post Go back to editing

Is 3V sufficient on pin DVDD_I/O(3.3V)_1 or we need atleast 3.3V

Thread Summary

The user is experiencing issues with the AD9910 IC not providing the required output when supplied with 3V at DVDD_I/O(3.3V)_1 and DVDD_I/O(3.3V)_2 pins. The final answer indicates that 3V is sufficient but performance is not guaranteed; it is recommended to use 3.3V for optimal operation.
AI Generated Content
Category: Hardware
Product Number: AD9910

My supply is providing 3V at DVDD_I/O(3.3V)_1 and DVDD_I/O(3.3V)_2 pins of AD9910 IC. 

But I'm not receiving required output. So is 3V sufficient or we need atleast 3.3 V at these pins for efficient operation.

Thanks.

Parents Reply Children
No Data