Post Go back to editing

AD9850 supply voltage range

Thread Summary

The user, a DFAE in Japan, inquired about the supply voltage range for AVDD and DVDD of the AD9850. The final answer confirmed that both should have the same tolerance as the 5V supply, which is 5V ±5%. The user also asked if ±5% is applicable for 3.3V, but this was not explicitly confirmed in the final answer.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD9850

Hello,

I'm a DFAE in Japan. Our customer want to know AD9850's supply voltage range of AVDD and DVDD. We only see "3.3 V or 5 V Single-Supply Operation" on the Data Sheet RevH.

Regards,

Hiroyuki

Thread Notes