Using AD5932, MCLK is 16.0MHz, and the DDS output is 2MHz, We are seeing the duty cycle is not 50% on the MSBOUT. We estimate 35% duty cycle. We are using DEC 2097152 as the FTW. We need 50% duty cycle on the MSBOUT pin. Are we missing something?
AD5932
Production
The AD5932 is a waveform generator offering a programmable frequency scan. Utilizing embedded digital processing that allows enhanced frequency control...
Datasheet
AD5932 on Analog.com
Using AD5932, MCLK is 16.0MHz, and the DDS output is 2MHz, We are seeing the duty cycle is not 50% on the MSBOUT. We estimate 35% duty cycle. We are using DEC 2097152 as the FTW. We need 50% duty cycle on the MSBOUT pin. Are we missing something?