Post Go back to editing

Is it possible to replace AD9952 for AD9951?

Thread Summary

The user inquired about replacing AD9951 with AD9952, noting the primary difference is the on-chip comparator. The final answer confirmed that the comparator can be powered down by setting CFR1[6]=1 to save power. The user then asked if connecting the comparator output to GND is acceptable, which was not directly addressed in the final answer.
AI Generated Content
Category: Hardware
Product Number: AD9952

Hi,

Let me ask you a basic question as below.

I suppose the difference between AD9951 and AD9952 is "comparator" only.

As this reason, it seems to be possilbe to replace AD9952 for AD9951.

Is my idea correct?

Thank you for your support.

Takumi

Thread Notes