Post Go back to editing

AD5933: Steep rise in phase

Thread Summary

The user observed steep rises in phase during impedance measurements with the AD5933 eval board, likely due to signal clipping at the power supply rails. The solution involves reducing the excitation voltage or RFB to prevent clipping, and monitoring the raw Re and Im data for accurate diagnostics. The AD5933's internal ADC and DFT can produce erroneous results if the sine wave is distorted, and using a 5x PGA gain can introduce additional clipping risks.
AI Generated Content
Category: Hardware
Product Number: AD5933

Hi all,

I'm using the AD5933 eval board in order to test an impedance measurement cell. I use shielded cables (30cm) to connect the cell with the board. The cell behaves like a capacitor.

I used the following settings for the measuerements:

Rfeedback: 1M
Rcal: 1M
Start frequency: 3kHz
Delta: 220Hz
511 points
Settling Time Cycles: 15
Upp Output: 1V
Gain: 1
Settling Time: X2
Multipoint Calibration

During my measurements i observed steep rises in the phase for which I had no explanation.

Because of this I installed a 10p capacitor instead of my measurement cell, but it shows a similar result:

Do you have got an explanation why the rise in the phase is that steep?

Thanks in advance!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.