I saw the reference design file CN0349 and CN0217, I think both are 2-wire implementation of the AD5P3x family IC. Can I get the circuit reference for the 4-wire implementation, with impedance range of 50 to 250 ohm.
Help will be highly appreciated.
AD5934
Production
The AD5934 is a high precision impedance converter system
solution that combines an on-board frequency generator with a 12-bit, 250 kSPS, analog-to-digital...
Datasheet
AD5934 on Analog.com
I saw the reference design file CN0349 and CN0217, I think both are 2-wire implementation of the AD5P3x family IC. Can I get the circuit reference for the 4-wire implementation, with impedance range of 50 to 250 ohm.
Help will be highly appreciated.
You may use this post as a starting point:
In the link, it is mentioned that setting Rcal = 20 can set the impedance range from 1 to 60. Can you please explain this, I did not get this. How can Rcal resistor set the range.
This is the result.
Yes, it would be great if you could find some 0.1% or better yet 0,05% resistors. Only avoid wire wound type - those may have too much inductance for AC measurements.
I did test and calibrate using different resistor values. I noted that the measurement accuracy is better near the calibrated resistance value. I think this is not a problem, this I can improve using some tricks.
The problem now I face, is, when I use 4 wires and short 2 wires together (T1 with R1 and T2 with R2) see the picture.
In this case I can get reading. See the pictures as a reference.
4 wires, 2 wires short together.

This is the waveform in the saline water.

But, WHEN I use for wires or electrodes separated from each other, then the behavior changes completely. I can not get any proper reading. please. check the pictures below.
This is 4 wires, first (white) and last (brown) are T1 and T2. Second (Blue) and third (black) are R1 and R2 (R stands for receiver)

This is the acquire waveform,

Saline water is used in both cases, with conductivity of 7.37 mS/cm.
Can you help with this.
Thanks
wires or electrodes separated from each other
I am not sure it is possible to separate the excitation wire Tn from the corresponding sensing wire Rn when in saline - it is going to break the DC working point of your circuit. Roughly speaking, the wires in saline are not galvanically connected to each other due to polarization layer forming at the interface. Very crudely, you can think of it as a capacitor between the wire surface and bulk saline, so the equivalent circuit approximating corresponding behavior would be something like this:
So, the sensing side of your circuit does not have any DC coupling to the rest of the circuit and your INAMP inputs are hanging at whatever voltage these capacitors are charged to by the input pin currents and leakages. On the excitation side this polarization "capacitance" would break the DC feedback loop for U2, that is why some kind of R11 is necessary.
I will add a capacitor on each Rn wires. This might block DC values.
The point is that, once wires are disconnected and put into the saline, the DC voltages are blocked by the equivalent capacitance of the polarization layer between the wire and electrolyte. Adding capacitors will put those in sequence with the polarization layer and will not help with the DC bias of the INAMP - the inputs would need to be DC-biased by some additional circuits. Connecting T1 to R1 and T2 to R2 takes care of the DC bias automatically, why would it be necessary to keep those wires apart?
the DC voltages are blocked by the equivalent capacitance of the polarization layer between the wire and electrolyte.
Got it,
But, I just went through the following link.
https://www.instructables.com/Body-Composition-using-BIA/
I did not found any additional circuit.
In this link adding capacitor is suggested on Rn wires.
But, I just went through the following link.
This link does not mention additional capacitors and nebulous enough showing a rectangle in place of "Body" and providing no information on the electrodes used.
But, I just went through the following link.
This link does not mention additional capacitors and nebulous enough showing a rectangle in place of "Body" and providing no information on the electrodes used.