I saw the reference design file CN0349 and CN0217, I think both are 2-wire implementation of the AD5P3x family IC. Can I get the circuit reference for the 4-wire implementation, with impedance range of 50 to 250 ohm.
Help will be highly appreciated.
AD5934
Production
The AD5934 is a high precision impedance converter system
solution that combines an on-board frequency generator with a 12-bit, 250 kSPS, analog-to-digital...
Datasheet
AD5934 on Analog.com
I saw the reference design file CN0349 and CN0217, I think both are 2-wire implementation of the AD5P3x family IC. Can I get the circuit reference for the 4-wire implementation, with impedance range of 50 to 250 ohm.
Help will be highly appreciated.
You may use this post as a starting point:
In the link, it is mentioned that setting Rcal = 20 can set the impedance range from 1 to 60. Can you please explain this, I did not get this. How can Rcal resistor set the range.
With this 4-wire circuit the output is directly proportional to the impedance under test.
Yes, I missed that point. Now I am getting 109 Ω when measuring 120 Ω.
The real component is 109.5 Ohms, which is a bit far from the expected 120 Ohm, but it could still be within manufacturing tolerance of both the resistors used for calibration and as the "unknown."
I ordered more resistors (different values) I will calibrate and measure a bunch of different resistors.
Thanks once again.
This is the result.
Yes, it would be great if you could find some 0.1% or better yet 0,05% resistors. Only avoid wire wound type - those may have too much inductance for AC measurements.
I did test and calibrate using different resistor values. I noted that the measurement accuracy is better near the calibrated resistance value. I think this is not a problem, this I can improve using some tricks.
The problem now I face, is, when I use 4 wires and short 2 wires together (T1 with R1 and T2 with R2) see the picture.
In this case I can get reading. See the pictures as a reference.
4 wires, 2 wires short together.

This is the waveform in the saline water.

But, WHEN I use for wires or electrodes separated from each other, then the behavior changes completely. I can not get any proper reading. please. check the pictures below.
This is 4 wires, first (white) and last (brown) are T1 and T2. Second (Blue) and third (black) are R1 and R2 (R stands for receiver)

This is the acquire waveform,

Saline water is used in both cases, with conductivity of 7.37 mS/cm.
Can you help with this.
Thanks
wires or electrodes separated from each other
I am not sure it is possible to separate the excitation wire Tn from the corresponding sensing wire Rn when in saline - it is going to break the DC working point of your circuit. Roughly speaking, the wires in saline are not galvanically connected to each other due to polarization layer forming at the interface. Very crudely, you can think of it as a capacitor between the wire surface and bulk saline, so the equivalent circuit approximating corresponding behavior would be something like this:
So, the sensing side of your circuit does not have any DC coupling to the rest of the circuit and your INAMP inputs are hanging at whatever voltage these capacitors are charged to by the input pin currents and leakages. On the excitation side this polarization "capacitance" would break the DC feedback loop for U2, that is why some kind of R11 is necessary.
I will add a capacitor on each Rn wires. This might block DC values.
The point is that, once wires are disconnected and put into the saline, the DC voltages are blocked by the equivalent capacitance of the polarization layer between the wire and electrolyte. Adding capacitors will put those in sequence with the polarization layer and will not help with the DC bias of the INAMP - the inputs would need to be DC-biased by some additional circuits. Connecting T1 to R1 and T2 to R2 takes care of the DC bias automatically, why would it be necessary to keep those wires apart?
the DC voltages are blocked by the equivalent capacitance of the polarization layer between the wire and electrolyte.
Got it,
But, I just went through the following link.
https://www.instructables.com/Body-Composition-using-BIA/
I did not found any additional circuit.
In this link adding capacitor is suggested on Rn wires.
In this link adding capacitor is suggested on Rn wires.
In this link adding capacitor is suggested on Rn wires.
Yes, but it does not explain what these capacitors are there for. It could be that the "body" is kept at some DC potential far different from Vdd/2, could be a requirement to DC-isolate the "body" from the circuit altogether (that could be the reason to also have the two more capacitors in the feedback loop of the OPAMP at the bottom of the diagram) or it could be that some non-polarizable electrodes were used (such as AgAgCl). If you want to follow this link - install all 4 capacitors and connect both INAMP inputs to the output of U3 with two larger resistors, 1MΩ or so. Thing to watch out with these 4 capacitors would be the wait time after Start Frequency command and before starting the measurements - this time should be long enough for the transients caused by these capacitors and resistors to settle and sine wave baseline to become stable.
I did solve the problem in simulation. I will test it on the PCB and I will post my results.
I noticed another strange behavior (maybe strange for me), the real and imaginary part have huge difference. See the picture below,
This is in the saline water, 2 wires are short together (T1 with R1 and T2 with R2).
What could be the reason.
Does your code convert these hex values to decimal? Imaginary value is negative, so it is max about 5 times larger than Real part. Not sure you need to worry about this difference as long as you can calibrate your system with a resistor and get reasonable results with an "unknown" resistor. When you connect resistor instead of saline, how different are the Re and Im values? Perhaps about the same?
I checked, real and imaginary value depends on the frequency in Hz, low input frequency give higher real value while higher input frequency gives higher imaginary values.
This is true for both resistor and saline (according to my test conditions).
Thanks
value depends on the frequency in Hz, low input frequency give higher real value while higher input frequency gives higher imaginary values.
How low and how high and at what clock frequency (MCLK)? The built-in "DFT" unit gives only approximation of the true DFT (in mathematical sense) and it is accurate enough only at higher frequencies and at a handful of frequencies when the chunk of sampled sine wave contains integer number of whole sinewave cycles fitting within the 1024-long sampling sequence.
Since a resistor does not have imaginary component in its impedance, one would expect all response to be found in Real register and Imaginary to be near zero. The reasons why the resistor response appears as a negative value in the Imaginary register are not explained in the documentation, but the good news is that it does not really matter as the calibration procedure eliminates this discrepancy by producing complex system gain (or system gain and system phase) which allows to arrive at the correct values when measuring the unknown impedance.
How low and how high and at what clock frequency (MCLK)? The built-in "DFT" unit gives only approximation of the true DFT (in mathematical sense) and it is accurate enough only at higher frequencies and at a handful of frequencies when the chunk of sampled sine wave contains integer number of whole sinewave cycles fitting within the 1024-long sampling sequence.
Sorry I was busy in something. Check the doc please. This is n saline water, start frequency 20k and 5k increments in each 15 steps.
00> 0:1:52 This is the start of the sweep function 00> 0:1:52 Frequency is 20000 00> 0:1:52 The real number is 6415 00> 0:1:52 The imag number is 61507 00> 0:1:52 Frequency is 25000 00> 0:1:52 The real number is 6793 00> 0:1:52 The imag number is 62908 00> 0:1:52 Frequency is 30000 00> 0:1:52 The real number is 6935 00> 0:1:52 The imag number is 64279 00> 0:1:52 Frequency is 35000 00> 0:1:52 The real number is 6874 00> 0:1:52 The imag number is 79 00> 0:1:52 Frequency is 40000 00> 0:1:52 The real number is 6581 00> 0:1:52 The imag number is 1363 00> 0:1:52 Frequency is 45000 00> 0:1:52 The real number is 6075 00> 0:1:52 The imag number is 2539 00> 0:1:52 Frequency is 50000 00> 0:1:52 The real number is 5372 00> 0:1:52 The imag number is 3606 00> 0:1:52 Frequency is 55000 00> 0:1:52 The real number is 4501 00> 0:1:52 The imag number is 4481 00> 0:1:52 Frequency is 60000 00> 0:1:52 The real number is 3518 00> 0:1:52 The imag number is 5187 00> 0:1:52 Frequency is 65000 00> 0:1:52 The real number is 2392 00> 0:1:52 The imag number is 5666 00> 0:1:52 Frequency is 70000 00> 0:1:52 The real number is 1228 00> 0:1:52 The imag number is 5937 00> 0:1:52 Frequency is 75000 00> 0:1:52 The real number is 51 00> 0:1:52 The imag number is 5962 00> 0:1:52 Frequency is 80000 00> 0:1:52 The real number is 64439 00> 0:1:52 The imag number is 5761 00> 0:1:52 Frequency is 85000 00> 0:1:52 The real number is 63372 00> 0:1:52 The imag number is 5349 00> 0:1:52 Frequency is 90000 00> 0:1:52 The real number is 62412 00> 0:1:52 The imag number is 4744 00> 0:1:52 This is the start of the sweep function 00> 0:1:52 Frequency is 20000 00> 0:1:52 The real number is 6415 00> 0:1:52 The imag number is 61506 00> 0:1:52 Frequency is 25000 00> 0:1:52 The real number is 6793 00> 0:1:52 The imag number is 62907 00> 0:1:52 Frequency is 30000 00> 0:1:52 The real number is 6940 00> 0:1:52 The imag number is 64270 00> 0:1:52 Frequency is 35000 00> 0:1:52 The real number is 6884 00> 0:1:52 The imag number is 77 00> 0:1:52 Frequency is 40000 00> 0:1:52 The real number is 6586 00> 0:1:52 The imag number is 1352 00> 0:1:52 Frequency is 45000 00> 0:1:52 The real number is 6085 00> 0:1:52 The imag number is 2542 00> 0:1:52 Frequency is 50000 00> 0:1:52 The real number is 5349 00> 0:1:52 The imag number is 3578 00> 0:1:52 Frequency is 55000 00> 0:1:52 The real number is 4505 00> 0:1:52 The imag number is 4480 00> 0:1:52 Frequency is 60000 00> 0:1:52 The real number is 3481 00> 0:1:52 The imag number is 5169 00> 0:1:52 Frequency is 65000 00> 0:1:52 The real number is 2391 00> 0:1:52 The imag number is 5662 00> 0:1:52 Frequency is 70000 00> 0:1:52 The real number is 1234 00> 0:1:52 The imag number is 5923 00> 0:1:52 Frequency is 75000 00> 0:1:52 The real number is 51 00> 0:1:52 The imag number is 5952 00> 0:1:52 Frequency is 80000 00> 0:1:52 The real number is 64442 00> 0:1:52 The imag number is 5760 00> 0:1:52 Frequency is 85000 00> 0:1:52 The real number is 63375 00> 0:1:52 The imag number is 5349 00> 0:1:52 Frequency is 90000 00> 0:1:52 The real number is 62424 00> 0:1:52 The imag number is 4741 00> 0:1:52 This is the start of the sweep function 00> 0:1:52 Frequency is 20000 00> 0:1:52 The real number is 6414 00> 0:1:52 The imag number is 61507 00> 0:1:52 Frequency is 25000 00> 0:1:52 The real number is 6790 00> 0:1:52 The imag number is 62903 00> 0:1:52 Frequency is 30000 00> 0:1:52 The real number is 6950 00> 0:1:52 The imag number is 64281 00> 0:1:52 Frequency is 35000 00> 0:1:52 The real number is 6877 00> 0:1:52 The imag number is 75 00> 0:1:52 Frequency is 40000 00> 0:1:52 The real number is 6594 00> 0:1:52 The imag number is 1357 00> 0:1:52 Frequency is 45000 00> 0:1:52 The real number is 6084 00> 0:1:52 The imag number is 2534 00> 0:1:52 Frequency is 50000 00> 0:1:52 The real number is 5349 00> 0:1:52 The imag number is 3579 00> 0:1:52 Frequency is 55000 00> 0:1:52 The real number is 4513 00> 0:1:52 The imag number is 4477 00> 0:1:52 Frequency is 60000 00> 0:1:52 The real number is 3490 00> 0:1:52 The imag number is 5199 00> 0:1:52 Frequency is 65000 00> 0:1:52 The real number is 2392 00> 0:1:52 The imag number is 5666 00> 0:1:52 Frequency is 70000 00> 0:1:52 The real number is 1233 00> 0:1:52 The imag number is 5924 00> 0:1:52 Frequency is 75000 00> 0:1:52 The real number is 52 00> 0:1:52 The imag number is 5952 00> 0:1:52 Frequency is 80000 00> 0:1:52 The real number is 64439 00> 0:1:52 The imag number is 5763 00> 0:1:52 Frequency is 85000 00> 0:1:52 The real number is 63372 00> 0:1:52 The imag number is 5350 00> 0:1:52 Frequency is 90000 00> 0:1:52 The real number is 62429 00> 0:1:52 The imag number is 4734 00> 0:1:52 This is the start of the sweep function 00> 0:1:52 Frequency is 20000 00> 0:1:52 The real number is 6415 00> 0:1:52 The imag number is 61505 00> 0:1:52 Frequency is 25000 00> 0:1:52 The real number is 6804 00> 0:1:52 The imag number is 62904 00> 0:1:52 Frequency is 30000 00> 0:1:52 The real number is 6947 00> 0:1:52 The imag number is 64270 00> 0:1:52 Frequency is 35000 00> 0:1:52 The real number is 6875 00> 0:1:52 The imag number is 77 00> 0:1:52 Frequency is 40000 00> 0:1:52 The real number is 6583 00> 0:1:52 The imag number is 1362 00> 0:1:52 Frequency is 45000 00> 0:1:52 The real number is 6085 00> 0:1:52 The imag number is 2541 00> 0:1:52 Frequency is 50000 00> 0:1:52 The real number is 5374 00> 0:1:52 The imag number is 3606 00> 0:1:52 Frequency is 55000 00> 0:1:52 The real number is 4506 00> 0:1:52 The imag number is 4481 00> 0:1:52 Frequency is 60000 00> 0:1:52 The real number is 3497 00> 0:1:52 The imag number is 5182 00> 0:1:52 Frequency is 65000 00> 0:1:52 The real number is 2392 00> 0:1:52 The imag number is 5664 00> 0:1:52 Frequency is 70000 00> 0:1:52 The real number is 1229 00> 0:1:52 The imag number is 5914 00> 0:1:52 Frequency is 75000 00> 0:1:52 The real number is 52 00> 0:1:52 The imag number is 5974 00> 0:1:52 Frequency is 80000 00> 0:1:52 The real number is 64440 00> 0:1:52 The imag number is 5757 00> 0:1:52 Frequency is 85000 00> 0:1:52 The real number is 63371 00> 0:1:52 The imag number is 5349 00> 0:1:52 Frequency is 90000 00> 0:1:52 The real number is 62418 00> 0:1:52 The imag number is 4748 00> 0:1:53 This is the start of the sweep function 00> 0:1:53 Frequency is 20000 00> 0:1:53 The real number is 6414 00> 0:1:53 The imag number is 61505 00> 0:1:53 Frequency is 25000 00> 0:1:53 The real number is 6794 00> 0:1:53 The imag number is 62905 00> 0:1:53 Frequency is 30000 00> 0:1:53 The real number is 6953 00> 0:1:53 The imag number is 64285 00> 0:1:53 Frequency is 35000 00> 0:1:53 The real number is 6875 00> 0:1:53 The imag number is 77 00> 0:1:53 Frequency is 40000 00> 0:1:53 The real number is 6597 00> 0:1:53 The imag number is 1359 00> 0:1:53 Frequency is 45000 00> 0:1:53 The real number is 6078 00> 0:1:53 The imag number is 2539 00> 0:1:53 Frequency is 50000 00> 0:1:53 The real number is 5364 00> 0:1:53 The imag number is 3628 00> 0:1:53 Frequency is 55000 00> 0:1:53 The real number is 4516 00> 0:1:53 The imag number is 4476 00> 0:1:53 Frequency is 60000 00> 0:1:53 The real number is 3510 00> 0:1:53 The imag number is 5162 00> 0:1:53 Frequency is 65000 00> 0:1:53 The real number is 2389 00> 0:1:53 The imag number is 5665 00> 0:1:53 Frequency is 70000 00> 0:1:53 The real number is 1229 00> 0:1:53 The imag number is 5939 00> 0:1:53 Frequency is 75000 00> 0:1:53 The real number is 51 00> 0:1:53 The imag number is 5964 00> 0:1:53 Frequency is 80000 00> 0:1:53 The real number is 64437 00> 0:1:53 The imag number is 5757 00> 0:1:53 Frequency is 85000 00> 0:1:53 The real number is 63371 00> 0:1:53 The imag number is 5350 00> 0:1:53 Frequency is 90000 00> 0:1:53 The real number is 62424 00> 0:1:53 The imag number is 4753 00> 0:1:53 This is the start of the sweep function 00> 0:1:53 Frequency is 20000 00> 0:1:53 The real number is 6414 00> 0:1:53 The imag number is 61504 00> 0:1:53 Frequency is 25000 00> 0:1:53 The real number is 6794 00> 0:1:53 The imag number is 62906 00> 0:1:53 Frequency is 30000 00> 0:1:53 The real number is 6951 00> 0:1:53 The imag number is 64280 00> 0:1:53 Frequency is 35000 00> 0:1:53 The real number is 6877 00> 0:1:53 The imag number is 79 00> 0:1:53 Frequency is 40000 00> 0:1:53 The real number is 6598 00> 0:1:53 The imag number is 1360 00> 0:1:53 Frequency is 45000 00> 0:1:53 The real number is 6078 00> 0:1:53 The imag number is 2539 00> 0:1:53 Frequency is 50000 00> 0:1:53 The real number is 5390 00> 0:1:53 The imag number is 3585 00> 0:1:53 Frequency is 55000 00> 0:1:53 The real number is 4506 00> 0:1:53 The imag number is 4481 00> 0:1:53 Frequency is 60000 00> 0:1:53 The real number is 3520 00> 0:1:53 The imag number is 5189 00> 0:1:53 Frequency is 65000 00> 0:1:53 The real number is 2394 00> 0:1:53 The imag number is 5667 00> 0:1:53 Frequency is 70000 00> 0:1:53 The real number is 1234 00> 0:1:53 The imag number is 5926 00> 0:1:53 Frequency is 75000 00> 0:1:53 The real number is 47 00> 0:1:53 The imag number is 5967 00> 0:1:53 Frequency is 80000 00> 0:1:53 The real number is 64439 00> 0:1:53 The imag number is 5763 00> 0:1:53 Frequency is 85000 00> 0:1:53 The real number is 63375 00> 0:1:53 The imag number is 5347 00> 0:1:53 Frequency is 90000 00> 0:1:53 The real number is 62412 00> 0:1:53 The imag number is 4744 00> 0:1:53 This is the start of the sweep function 00> 0:1:53 Frequency is 20000 00> 0:1:53 The real number is 6415 00> 0:1:53 The imag number is 61505 00> 0:1:53 Frequency is 25000 00> 0:1:53 The real number is 6788 00> 0:1:53 The imag number is 62897 00> 0:1:53 Frequency is 30000 00> 0:1:53 The real number is 6947 00> 0:1:53 The imag number is 64270 00> 0:1:53 Frequency is 35000 00> 0:1:53 The real number is 6876 00> 0:1:53 The imag number is 77 00> 0:1:53 Frequency is 40000 00> 0:1:53 The real number is 6589 00> 0:1:53 The imag number is 1347 00> 0:1:53 Frequency is 45000 00> 0:1:53 The real number is 6087 00> 0:1:53 The imag number is 2542 00> 0:1:53 Frequency is 50000 00> 0:1:53 The real number is 5367 00> 0:1:53 The imag number is 3621 00> 0:1:53 Frequency is 55000 00> 0:1:53 The real number is 4517 00> 0:1:53 The imag number is 4476 00> 0:1:53 Frequency is 60000 00> 0:1:53 The real number is 3520 00> 0:1:53 The imag number is 5188 00> 0:1:53 Frequency is 65000 00> 0:1:53 The real number is 2392 00> 0:1:53 The imag number is 5670 00> 0:1:53 Frequency is 70000 00> 0:1:53 The real number is 1233 00> 0:1:53 The imag number is 5926 00> 0:1:53 Frequency is 75000 00> 0:1:53 The real number is 53 00> 0:1:53 The imag number is 5964 00> 0:1:53 Frequency is 80000 00> 0:1:53 The real number is 64432 00> 0:1:53 The imag number is 5769 00> 0:1:53 Frequency is 85000 00> 0:1:53 The real number is 63374 00> 0:1:53 The imag number is 5351 00> 0:1:53 Frequency is 90000 00> 0:1:53 The real number is 62418 00> 0:1:53 The imag number is 4748 00> 0:1:54 This is the start of the sweep function 00> 0:1:54 Frequency is 20000 00> 0:1:54 The real number is 6415 00> 0:1:54 The imag number is 61505 00> 0:1:54 Frequency is 25000 00> 0:1:54 The real number is 6794 00> 0:1:54 The imag number is 62906 00> 0:1:54 Frequency is 30000 00> 0:1:54 The real number is 6941 00> 0:1:54 The imag number is 64270 00> 0:1:54 Frequency is 35000 00> 0:1:54 The real number is 6885 00> 0:1:54 The imag number is 77 00> 0:1:54 Frequency is 40000 00> 0:1:54 The real number is 6588 00> 0:1:54 The imag number is 1352 00> 0:1:54 Frequency is 45000 00> 0:1:54 The real number is 6086 00> 0:1:54 The imag number is 2538 00> 0:1:54 Frequency is 50000 00> 0:1:54 The real number is 5366 00> 0:1:54 The imag number is 3619 00> 0:1:54 Frequency is 55000 00> 0:1:54 The real number is 4505 00> 0:1:54 The imag number is 4481 00> 0:1:54 Frequency is 60000 00> 0:1:54 The real number is 3497 00> 0:1:54 The imag number is 5182 00> 0:1:54 Frequency is 65000 00> 0:1:54 The real number is 2391 00> 0:1:54 The imag number is 5664 00> 0:1:54 Frequency is 70000 00> 0:1:54 The real number is 1228 00> 0:1:54 The imag number is 5911 00> 0:1:54 Frequency is 75000 00> 0:1:54 The real number is 48 00> 0:1:54 The imag number is 5960 00> 0:1:54 Frequency is 80000 00> 0:1:54 The real number is 64438 00> 0:1:54 The imag number is 5763 00> 0:1:54 Frequency is 85000 00> 0:1:54 The real number is 63371 00> 0:1:54 The imag number is 5350 00> 0:1:54 Frequency is 90000 00> 0:1:54 The real number is 62418 00> 0:1:54 The imag number is 4746 00> 0:1:54 This is the start of the sweep function 00> 0:1:54 Frequency is 20000 00> 0:1:54 The real number is 6415 00> 0:1:54 The imag number is 61506 00> 0:1:54 Frequency is 25000 00> 0:1:54 The real number is 6794 00> 0:1:54 The imag number is 62905 00> 0:1:54 Frequency is 30000 00> 0:1:54 The real number is 6953 00> 0:1:54 The imag number is 64287 00> 0:1:54 Frequency is 35000 00> 0:1:54 The real number is 6878 00> 0:1:54 The imag number is 76 00> 0:1:54 Frequency is 40000 00> 0:1:54 The real number is 6581 00> 0:1:54 The imag number is 1363 00> 0:1:54 Frequency is 45000 00> 0:1:54 The real number is 6086 00> 0:1:54 The imag number is 2538 00> 0:1:54 Frequency is 50000 00> 0:1:54 The real number is 5363 00> 0:1:54 The imag number is 3630 00> 0:1:54 Frequency is 55000 00> 0:1:54 The real number is 4504 00> 0:1:54 The imag number is 4480 00> 0:1:54 Frequency is 60000 00> 0:1:54 The real number is 3480 00> 0:1:54 The imag number is 5170 00> 0:1:54 Frequency is 65000 00> 0:1:54 The real number is 2390 00> 0:1:54 The imag number is 5663 00> 0:1:54 Frequency is 70000 00> 0:1:54 The real number is 1227 00> 0:1:54 The imag number is 5938 00> 0:1:54 Frequency is 75000 00> 0:1:54 The real number is 42 00> 0:1:54 The imag number is 5947 00> 0:1:54 Frequency is 80000 00> 0:1:54 The real number is 64432 00> 0:1:54 The imag number is 5770 00> 0:1:54 Frequency is 85000 00> 0:1:54 The real number is 63374 00> 0:1:54 The imag number is 5346 00> 0:1:54 Frequency is 90000 00> 0:1:54 The real number is 62411 00> 0:1:54 The imag number is 4744 00> 0:1:54 This is the start of the sweep function 00> 0:1:54 Frequency is 20000 00> 0:1:54 The real number is 6414 00> 0:1:54 The imag number is 61506 00> 0:1:54 Frequency is 25000 00> 0:1:54 The real number is 6794 00> 0:1:54 The imag number is 62907 00> 0:1:54 Frequency is 30000 00> 0:1:54 The real number is 6952 00> 0:1:54 The imag number is 64287 00> 0:1:54 Frequency is 35000 00> 0:1:54 The real number is 6876 00> 0:1:54 The imag number is 82 00> 0:1:54 Frequency is 40000 00> 0:1:54 The real number is 6580 00> 0:1:54 The imag number is 1363 00> 0:1:54 Frequency is 45000 00> 0:1:54 The real number is 6083 00> 0:1:54 The imag number is 2543 00> 0:1:54 Frequency is 50000 00> 0:1:54 The real number is 5347 00> 0:1:54 The imag number is 3579 00> 0:1:54 Frequency is 55000 00> 0:1:54 The real number is 4511 00> 0:1:54 The imag number is 4478 00> 0:1:54 Frequency is 60000 00> 0:1:54 The real number is 3489 00> 0:1:54 The imag number is 5199 00> 0:1:54 Frequency is 65000 00> 0:1:54 The real number is 2389 00> 0:1:54 The imag number is 5661 00> 0:1:54 Frequency is 70000 00> 0:1:54 The real number is 1226 00> 0:1:54 The imag number is 5922 00> 0:1:54 Frequency is 75000 00> 0:1:54 The real number is 50 00> 0:1:54 The imag number is 5950 00> 0:1:54 Frequency is 80000 00> 0:1:54 The real number is 64442 00> 0:1:54 The imag number is 5756 00> 0:1:54 Frequency is 85000 00> 0:1:54 The real number is 63374 00> 0:1:54 The imag number is 5348 00> 0:1:54 Frequency is 90000 00> 0:1:54 The real number is 62430 00> 0:1:54 The imag number is 4746 00> 0:1:54 This is the start of the sweep function 00> 0:1:54 Frequency is 20000 00> 0:1:54 The real number is 6415 00> 0:1:54 The imag number is 61508 00> 0:1:54 Frequency is 25000 00> 0:1:54 The real number is 6794 00> 0:1:54 The imag number is 62907 00> 0:1:54 Frequency is 30000 00> 0:1:54 The real number is 6951 00> 0:1:54 The imag number is 64287 00> 0:1:54 Frequency is 35000 00> 0:1:54 The real number is 6876 00> 0:1:54 The imag number is 77 00> 0:1:54 Frequency is 40000 00> 0:1:54 The real number is 6585 00> 0:1:54 The imag number is 1354 00> 0:1:54 Frequency is 45000 00> 0:1:54 The real number is 6075 00> 0:1:54 The imag number is 2540 00> 0:1:54 Frequency is 50000 00> 0:1:54 The real number is 5375 00> 0:1:54 The imag number is 3618 00> 0:1:54 Frequency is 55000 00> 0:1:54 The real number is 4500 00> 0:1:54 The imag number is 4482 00> 0:1:54 Frequency is 60000 00> 0:1:54 The real number is 3507 00> 0:1:54 The imag number is 5174 00> 0:1:54 Frequency is 65000 00> 0:1:54 The real number is 2389 00> 0:1:54 The imag number is 5669 00> 0:1:54 Frequency is 70000 00> 0:1:54 The real number is 1232 00> 0:1:54 The imag number is 5923 00> 0:1:54 Frequency is 75000 00> 0:1:54 The real number is 47 00> 0:1:54 The imag number is 5958 00> 0:1:54 Frequency is 80000 00> 0:1:54 The real number is 64447 00> 0:1:54 The imag number is 5757 00> 0:1:54 Frequency is 85000 00> 0:1:54 The real number is 63372 00> 0:1:54 The imag number is 5347 00> 0:1:54 Frequency is 90000 00> 0:1:54 The real number is 62417 00> 0:1:54 The imag number is 4746 00> 0:1:55 This is the start of the sweep function 00> 0:1:55 Frequency is 20000 00> 0:1:55 The real number is 6415 00> 0:1:55 The imag number is 61508 00> 0:1:55 Frequency is 25000 00> 0:1:55 The real number is 6803 00> 0:1:55 The imag number is 62905 00> 0:1:55 Frequency is 30000 00> 0:1:55 The real number is 6950 00> 0:1:55 The imag number is 64276 00> 0:1:55 Frequency is 35000 00> 0:1:55 The real number is 6883 00> 0:1:55 The imag number is 79 00> 0:1:55 Frequency is 40000 00> 0:1:55 The real number is 6582 00> 0:1:55 The imag number is 1356 00> 0:1:55 Frequency is 45000 00> 0:1:55 The real number is 6082 00> 0:1:55 The imag number is 2538 00> 0:1:55 Frequency is 50000 00> 0:1:55 The real number is 5361 00> 0:1:55 The imag number is 3630 00> 0:1:55 Frequency is 55000 00> 0:1:55 The real number is 4499 00> 0:1:55 The imag number is 4481 00> 0:1:55 Frequency is 60000 00> 0:1:55 The real number is 3489 00> 0:1:55 The imag number is 5198 00> 0:1:55 Frequency is 65000 00> 0:1:55 The real number is 2389 00> 0:1:55 The imag number is 5661 00> 0:1:55 Frequency is 70000 00> 0:1:55 The real number is 1225 00> 0:1:55 The imag number is 5922 00> 0:1:55 Frequency is 75000 00> 0:1:55 The real number is 49 00> 0:1:55 The imag number is 5964 00> 0:1:55 Frequency is 80000 00> 0:1:55 The real number is 64437 00> 0:1:55 The imag number is 5760 00> 0:1:55 Frequency is 85000 00> 0:1:55 The real number is 63374 00> 0:1:55 The imag number is 5344 00> 0:1:55 Frequency is 90000 00> 0:1:55 The real number is 62425 00> 0:1:55 The imag number is 4752 00> 0:1:55 This is the start of the sweep function 00> 0:1:55 Frequency is 20000 00> 0:1:55 The real number is 6415 00> 0:1:55 The imag number is 61508 00> 0:1:55 Frequency is 25000 00> 0:1:55 The real number is 6791 00> 0:1:55 The imag number is 62905 00> 0:1:55 Frequency is 30000 00> 0:1:55 The real number is 6939 00> 0:1:55 The imag number is 64273 00> 0:1:55 Frequency is 35000 00> 0:1:55 The real number is 6877 00> 0:1:55 The imag number is 77 00> 0:1:55 Frequency is 40000 00> 0:1:55 The real number is 6586 00> 0:1:55 The imag number is 1353 00> 0:1:55 Frequency is 45000 00> 0:1:55 The real number is 6082 00> 0:1:55 The imag number is 2543 00> 0:1:55 Frequency is 50000 00> 0:1:55 The real number is 5372 00> 0:1:55 The imag number is 3608 00> 0:1:55 Frequency is 55000 00> 0:1:55 The real number is 4510 00> 0:1:55 The imag number is 4478 00> 0:1:55 Frequency is 60000 00> 0:1:55 The real number is 3506 00> 0:1:55 The imag number is 5161 00> 0:1:55 Frequency is 65000 00> 0:1:55 The real number is 2390 00> 0:1:55 The imag number is 5665 00> 0:1:55 Frequency is 70000 00> 0:1:55 The real number is 1225 00> 0:1:55 The imag number is 5922 00> 0:1:55 Frequency is 75000 00> 0:1:55 The real number is 44 00> 0:1:55 The imag number is 5954 00> 0:1:55 Frequency is 80000 00> 0:1:55 The real number is 64441 00> 0:1:55 The imag number is 5753 00> 0:1:55 Frequency is 85000 00> 0:1:55 The real number is 63371 00> 0:1:55 The imag number is 5348 00> 0:1:55 Frequency is 90000 00> 0:1:55 The real number is 62412 00> 0:1:55 The imag number is 4740 00> 0:1:55 This is the start of the sweep function 00> 0:1:55 Frequency is 20000 00> 0:1:55 The real number is 6415 00> 0:1:55 The imag number is 61508 00> 0:1:55 Frequency is 25000 00> 0:1:55 The real number is 6794 00> 0:1:55 The imag number is 62907 00> 0:1:55 Frequency is 30000 00> 0:1:55 The real number is 6951 00> 0:1:55 The imag number is 64276 00> 0:1:55 Frequency is 35000 00> 0:1:55 The real number is 6874 00> 0:1:55 The imag number is 83 00> 0:1:55 Frequency is 40000 00> 0:1:55 The real number is 6582 00> 0:1:55 The imag number is 1364 00> 0:1:55 Frequency is 45000 00> 0:1:55 The real number is 6075 00> 0:1:55 The imag number is 2540 00> 0:1:55 Frequency is 50000 00> 0:1:55 The real number is 5331 00> 0:1:55 The imag number is 3601 00> 0:1:55 Frequency is 55000 00> 0:1:55 The real number is 4502 00> 0:1:55 The imag number is 4480 00> 0:1:55 Frequency is 60000 00> 0:1:55 The real number is 3505 00> 0:1:55 The imag number is 5160 00> 0:1:55 Frequency is 65000 00> 0:1:55 The real number is 2388 00> 0:1:55 The imag number is 5669 00> 0:1:55 Frequency is 70000 00> 0:1:55 The real number is 1226 00> 0:1:55 The imag number is 5911 00> 0:1:55 Frequency is 75000 00> 0:1:55 The real number is 49 00> 0:1:55 The imag number is 5960 00> 0:1:55 Frequency is 80000 00> 0:1:55 The real number is 64440 00> 0:1:55 The imag number is 5753 00> 0:1:55 Frequency is 85000 00> 0:1:55 The real number is 63371 00> 0:1:55 The imag number is 5347 00> 0:1:55 Frequency is 90000 00> 0:1:55 The real number is 62430 00> 0:1:55 The imag number is 4731 00> 0:1:56 This is the start of the sweep function 00> 0:1:56 Frequency is 20000 00> 0:1:56 The real number is 6415 00> 0:1:56 The imag number is 61508 00> 0:1:56 Frequency is 25000 00> 0:1:56 The real number is 6804 00> 0:1:56 The imag number is 62906 00> 0:1:56 Frequency is 30000 00> 0:1:56 The real number is 6950 00> 0:1:56 The imag number is 64276 00> 0:1:56 Frequency is 35000 00> 0:1:56 The real number is 6877 00> 0:1:56 The imag number is 77 00> 0:1:56 Frequency is 40000 00> 0:1:56 The real number is 6580 00> 0:1:56 The imag number is 1365 00> 0:1:56 Frequency is 45000 00> 0:1:56 The real number is 6082 00> 0:1:56 The imag number is 2536 00> 0:1:56 Frequency is 50000 00> 0:1:56 The real number is 5376 00> 0:1:56 The imag number is 3611 00> 0:1:56 Frequency is 55000 00> 0:1:56 The real number is 4513 00> 0:1:56 The imag number is 4476 00> 0:1:56 Frequency is 60000 00> 0:1:56 The real number is 3495 00> 0:1:56 The imag number is 5181 00> 0:1:56 Frequency is 65000 00> 0:1:56 The real number is 2385 00> 0:1:56 The imag number is 5664 00> 0:1:56 Frequency is 70000 00> 0:1:56 The real number is 1227 00> 0:1:56 The imag number is 5912 00> 0:1:56 Frequency is 75000 00> 0:1:56 The real number is 46 00> 0:1:56 The imag number is 5963 00> 0:1:56 Frequency is 80000 00> 0:1:56 The real number is 64432 00> 0:1:56 The imag number is 5766 00> 0:1:56 Frequency is 85000 00> 0:1:56 The real number is 63374 00> 0:1:56 The imag number is 5344 00> 0:1:56 Frequency is 90000 00> 0:1:56 The real number is 62422 00> 0:1:56 The imag number is 4751 00> 0:1:56 This is the start of the sweep function 00> 0:1:56 Frequency is 20000 00> 0:1:56 The real number is 6414 00> 0:1:56 The imag number is 61508 00> 0:1:56 Frequency is 25000 00> 0:1:56 The real number is 6788 00> 0:1:56 The imag number is 62899 00> 0:1:56 Frequency is 30000 00> 0:1:56 The real number is 6952 00> 0:1:56 The imag number is 64288 00> 0:1:56 Frequency is 35000 00> 0:1:56 The real number is 6877 00> 0:1:56 The imag number is 78 00> 0:1:56 Frequency is 40000 00> 0:1:56 The real number is 6587 00> 0:1:56 The imag number is 1349 00> 0:1:56 Frequency is 45000 00> 0:1:56 The real number is 6084 00> 0:1:56 The imag number is 2544 00> 0:1:56 Frequency is 50000 00> 0:1:56 The real number is 5388 00> 0:1:56 The imag number is 3587 00> 0:1:56 Frequency is 55000 00> 0:1:56 The real number is 4502 00> 0:1:56 The imag number is 4481 00> 0:1:56 Frequency is 60000 00> 0:1:56 The real number is 3507 00> 0:1:56 The imag number is 5175 00> 0:1:56 Frequency is 65000 00> 0:1:56 The real number is 2386 00> 0:1:56 The imag number is 5663 00> 0:1:56 Frequency is 70000 00> 0:1:56 The real number is 1218 00> 0:1:56 The imag number is 5923 00> 0:1:56 Frequency is 75000 00> 0:1:56 The real number is 48 00> 0:1:56 The imag number is 5960 00> 0:1:56 Frequency is 80000 00> 0:1:56 The real number is 64431 00> 0:1:56 The imag number is 5768 00> 0:1:56 Frequency is 85000 00> 0:1:56 The real number is 63373 00> 0:1:56 The imag number is 5344 00> 0:1:56 Frequency is 90000 00> 0:1:56 The real number is 62416 00> 0:1:56 The imag number is 4745 00> 0:1:56 This is the start of the sweep function 00> 0:1:56 Frequency is 20000 00> 0:1:56 The real number is 6416 00> 0:1:56 The imag number is 61506 00> 0:1:56 Frequency is 25000 00> 0:1:56 The real number is 6794 00> 0:1:56 The imag number is 62906 00> 0:1:56 Frequency is 30000 00> 0:1:56 The real number is 6951 00> 0:1:56 The imag number is 64282 00> 0:1:56 Frequency is 35000 00> 0:1:56 The real number is 6878 00> 0:1:56 The imag number is 77 00> 0:1:56 Frequency is 40000 00> 0:1:56 The real number is 6583 00> 0:1:56 The imag number is 1365 00> 0:1:56 Frequency is 45000 00> 0:1:56 The real number is 6084 00> 0:1:56 The imag number is 2544 00> 0:1:56 Frequency is 50000 00> 0:1:56 The real number is 5388 00> 0:1:56 The imag number is 3586 00> 0:1:56 Frequency is 55000 00> 0:1:56 The real number is 4514 00> 0:1:56 The imag number is 4476 00> 0:1:56 Frequency is 60000 00> 0:1:56 The real number is 3489 00> 0:1:56 The imag number is 5200 00> 0:1:56 Frequency is 65000 00> 0:1:56 The real number is 2386 00> 0:1:56 The imag number is 5664 00> 0:1:56 Frequency is 70000 00> 0:1:56 The real number is 1224 00> 0:1:56 The imag number is 5937 00> 0:1:56 Frequency is 75000 00> 0:1:56 The real number is 46 00> 0:1:56 The imag number is 5957 00> 0:1:56 Frequency is 80000 00> 0:1:56 The real number is 64439 00> 0:1:56 The imag number is 5755 00> 0:1:56 Frequency is 85000 00> 0:1:56 The real number is 63374 00> 0:1:56 The imag number is 5345 00> 0:1:56 Frequency is 90000 00> 0:1:56 The real number is 62428 00> 0:1:56 The imag number is 4745 00> 0:1:56 This is the start of the sweep function 00> 0:1:56 Frequency is 20000 00> 0:1:56 The real number is 6415 00> 0:1:56 The imag number is 61507 00> 0:1:56 Frequency is 25000 00> 0:1:56 The real number is 6795 00> 0:1:56 The imag number is 62909 00> 0:1:56 Frequency is 30000 00> 0:1:56 The real number is 6952 00> 0:1:56 The imag number is 64282 00> 0:1:56 Frequency is 35000 00> 0:1:56 The real number is 6874 00> 0:1:56 The imag number is 79 00> 0:1:56 Frequency is 40000 00> 0:1:56 The real number is 6580 00> 0:1:56 The imag number is 1356 00> 0:1:56 Frequency is 45000 00> 0:1:56 The real number is 6083 00> 0:1:56 The imag number is 2535 00> 0:1:56 Frequency is 50000 00> 0:1:56 The real number is 5373 00> 0:1:56 The imag number is 3608 00> 0:1:56 Frequency is 55000 00> 0:1:56 The real number is 4513 00> 0:1:56 The imag number is 4476 00> 0:1:56 Frequency is 60000 00> 0:1:56 The real number is 3497 00> 0:1:56 The imag number is 5181 00> 0:1:56 Frequency is 65000 00> 0:1:56 The real number is 2390 00> 0:1:56 The imag number is 5663 00> 0:1:56 Frequency is 70000 00> 0:1:56 The real number is 1228 00> 0:1:56 The imag number is 5930 00> 0:1:56 Frequency is 75000 00> 0:1:56 The real number is 49 00> 0:1:56 The imag number is 5961 00> 0:1:56 Frequency is 80000 00> 0:1:56 The real number is 64429 00> 0:1:56 The imag number is 5763 00> 0:1:56 Frequency is 85000 00> 0:1:56 The real number is 63371 00> 0:1:56 The imag number is 5347 00> 0:1:56 Frequency is 90000 00> 0:1:56 The real number is 62421 00> 0:1:56 The imag number is 4752 00> 0:1:57 This is the start of the sweep function 00> 0:1:57 Frequency is 20000 00> 0:1:57 The real number is 6416 00> 0:1:57 The imag number is 61505 00> 0:1:57 Frequency is 25000 00> 0:1:57 The real number is 6805 00> 0:1:57 The imag number is 62905 00> 0:1:57 Frequency is 30000 00> 0:1:57 The real number is 6947 00> 0:1:57 The imag number is 64272 00> 0:1:57 Frequency is 35000 00> 0:1:57 The real number is 6886 00> 0:1:57 The imag number is 79 00> 0:1:57 Frequency is 40000 00> 0:1:57 The real number is 6590 00> 0:1:57 The imag number is 1350 00> 0:1:57 Frequency is 45000 00> 0:1:57 The real number is 6076 00> 0:1:57 The imag number is 2540 00> 0:1:57 Frequency is 50000 00> 0:1:57 The real number is 5362 00> 0:1:57 The imag number is 3630 00> 0:1:57 Frequency is 55000 00> 0:1:57 The real number is 4511 00> 0:1:57 The imag number is 4479 00> 0:1:57 Frequency is 60000 00> 0:1:57 The real number is 3497 00> 0:1:57 The imag number is 5183 00> 0:1:57 Frequency is 65000 00> 0:1:57 The real number is 2390 00> 0:1:57 The imag number is 5670 00> 0:1:57 Frequency is 70000 00> 0:1:57 The real number is 1232 00> 0:1:57 The imag number is 5925 00> 0:1:57 Frequency is 75000 00> 0:1:57 The real number is 50 00> 0:1:57 The imag number is 5952 00> 0:1:57 Frequency is 80000 00> 0:1:57 The real number is 64431 00> 0:1:57 The imag number is 5763 00> 0:1:57 Frequency is 85000 00> 0:1:57 The real number is 63374 00> 0:1:57 The imag number is 5344 00> 0:1:57 Frequency is 90000 00> 0:1:57 The real number is 62423 00> 0:1:57 The imag number is 4741 00> 0:1:57 This is the start of the sweep function 00> 0:1:57 Frequency is 20000 00> 0:1:57 The real number is 6417 00> 0:1:57 The imag number is 61507 00> 0:1:57 Frequency is 25000 00> 0:1:57 The real number is 6796 00> 0:1:57 The imag number is 62906 00> 0:1:57 Frequency is 30000 00> 0:1:57 The real number is 6947 00> 0:1:57 The imag number is 64272 00> 0:1:57 Frequency is 35000 00> 0:1:57 The real number is 6879 00> 0:1:57 The imag number is 77 00> 0:1:57 Frequency is 40000 00> 0:1:57 The real number is 6580 00> 0:1:57 The imag number is 1355 00> 0:1:57 Frequency is 45000 00> 0:1:57 The real number is 6086 00> 0:1:57 The imag number is 2539 00> 0:1:57 Frequency is 50000 00> 0:1:57 The real number is 5388 00> 0:1:57 The imag number is 3586 00> 0:1:57 Frequency is 55000 00> 0:1:57 The real number is 4503 00> 0:1:57 The imag number is 4481 00> 0:1:57 Frequency is 60000 00> 0:1:57 The real number is 3508 00> 0:1:57 The imag number is 5176 00> 0:1:57 Frequency is 65000 00> 0:1:57 The real number is 2390 00> 0:1:57 The imag number is 5671 00> 0:1:57 Frequency is 70000 00> 0:1:57 The real number is 1226 00> 0:1:57 The imag number is 5924 00> 0:1:57 Frequency is 75000 00> 0:1:57 The real number is 48 00> 0:1:57 The imag number is 5964 00> 0:1:57 Frequency is 80000 00> 0:1:57 The real number is 64442 00> 0:1:57 The imag number is 5758 00> 0:1:57 Frequency is 85000 00> 0:1:57 The real number is 63374 00> 0:1:57 The imag number is 5348 00> 0:1:57 Frequency is 90000 00> 0:1:57 The real number is 62428 00> 0:1:57 The imag number is 4734 00> 0:1:57 This is the start of the sweep function 00> 0:1:57 Frequency is 20000 00> 0:1:57 The real number is 6416 00> 0:1:57 The imag number is 61507 00> 0:1:57 Frequency is 25000 00> 0:1:57 The real number is 6789 00> 0:1:57 The imag number is 62898 00> 0:1:57 Frequency is 30000 00> 0:1:57 The real number is 6937 00> 0:1:57 The imag number is 64279 00> 0:1:57 Frequency is 35000 00> 0:1:57 The real number is 6876 00> 0:1:57 The imag number is 79 00> 0:1:57 Frequency is 40000 00> 0:1:57 The real number is 6582 00> 0:1:57 The imag number is 1364 00> 0:1:57 Frequency is 45000 00> 0:1:57 The real number is 6083 00> 0:1:57 The imag number is 2536 00> 0:1:57 Frequency is 50000 00> 0:1:57 The real number is 5389 00> 0:1:57 The imag number is 3587 00> 0:1:57 Frequency is 55000 00> 0:1:57 The real number is 4500 00> 0:1:57 The imag number is 4483 00> 0:1:57 Frequency is 60000 00> 0:1:57 The real number is 3479 00> 0:1:57 The imag number is 5171 00> 0:1:57 Frequency is 65000 00> 0:1:57 The real number is 2387 00> 0:1:57 The imag number is 5666 00> 0:1:57 Frequency is 70000 00> 0:1:57 The real number is 1214 00> 0:1:57 The imag number is 5926 00> 0:1:57 Frequency is 75000 00> 0:1:57 The real number is 52 00> 0:1:57 The imag number is 5962 00> 0:1:57 Frequency is 80000 00> 0:1:57 The real number is 64446 00> 0:1:57 The imag number is 5760 00> 0:1:57 Frequency is 85000 00> 0:1:57 The real number is 63370 00> 0:1:57 The imag number is 5347 00> 0:1:57 Frequency is 90000 00> 0:1:57 The real number is 62424 00> 0:1:57 The imag number is 4753 00> 0:1:58 This is the start of the sweep function 00> 0:1:58 Frequency is 20000 00> 0:1:58 The real number is 6417 00> 0:1:58 The imag number is 61507 00> 0:1:58 Frequency is 25000 00> 0:1:58 The real number is 6805 00> 0:1:58 The imag number is 62906 00> 0:1:58 Frequency is 30000 00> 0:1:58 The real number is 6951 00> 0:1:58 The imag number is 64281 00> 0:1:58 Frequency is 35000 00> 0:1:58 The real number is 6877 00> 0:1:58 The imag number is 82 00> 0:1:58 Frequency is 40000 00> 0:1:58 The real number is 6585 00> 0:1:58 The imag number is 1365 00> 0:1:58 Frequency is 45000 00> 0:1:58 The real number is 6077 00> 0:1:58 The imag number is 2540 00> 0:1:58 Frequency is 50000 00> 0:1:58 The real number is 5374 00> 0:1:58 The imag number is 3608 00> 0:1:58 Frequency is 55000 00> 0:1:58 The real number is 4512 00> 0:1:58 The imag number is 4479 00> 0:1:58 Frequency is 60000 00> 0:1:58 The real number is 3497 00> 0:1:58 The imag number is 5181 00> 0:1:58 Frequency is 65000 00> 0:1:58 The real number is 2387 00> 0:1:58 The imag number is 5664 00> 0:1:58 Frequency is 70000 00> 0:1:58 The real number is 1232 00> 0:1:58 The imag number is 5925 00> 0:1:58 Frequency is 75000 00> 0:1:58 The real number is 49 00> 0:1:58 The imag number is 5961 00> 0:1:58 Frequency is 80000 00> 0:1:58 The real number is 64442 00> 0:1:58 The imag number is 5762 00> 0:1:58 Frequency is 85000 00> 0:1:58 The real number is 63370 00> 0:1:58 The imag number is 5348 00> 0:1:58 Frequency is 90000 00> 0:1:58 The real number is 62423 00> 0:1:58 The imag number is 4742 00> 0:1:58 This is the start of the sweep function 00> 0:1:58 Frequency is 20000 00> 0:1:58 The real number is 6415 00> 0:1:58 The imag number is 61505 00> 0:1:58 Frequency is 25000 00> 0:1:58 The real number is 6789 00> 0:1:58 The imag number is 62898 00> 0:1:58 Frequency is 30000 00> 0:1:58 The real number is 6953 00> 0:1:58 The imag number is 64274 00> 0:1:58 Frequency is 35000 00> 0:1:58 The real number is 6877 00> 0:1:58 The imag number is 82 00> 0:1:58 Frequency is 40000 00> 0:1:58 The real number is 6583 00> 0:1:58 The imag number is 1365 00> 0:1:58 Frequency is 45000 00> 0:1:58 The real number is 6086 00> 0:1:58 The imag number is 2544 00> 0:1:58 Frequency is 50000 00> 0:1:58 The real number is 5349 00> 0:1:58 The imag number is 3582 00> 0:1:58 Frequency is 55000 00> 0:1:58 The real number is 4515 00> 0:1:58 The imag number is 4477 00> 0:1:58 Frequency is 60000 00> 0:1:58 The real number is 3497 00> 0:1:58 The imag number is 5183 00> 0:1:58 Frequency is 65000 00> 0:1:58 The real number is 2391 00> 0:1:58 The imag number is 5671 00> 0:1:58 Frequency is 70000 00> 0:1:58 The real number is 1232 00> 0:1:58 The imag number is 5925 00> 0:1:58 Frequency is 75000 00> 0:1:58 The real number is 41 00> 0:1:58 The imag number is 5947 00> 0:1:58 Frequency is 80000 00> 0:1:58 The real number is 64440 00> 0:1:58 The imag number is 5758 00> 0:1:58 Frequency is 85000 00> 0:1:58 The real number is 63370 00> 0:1:58 The imag number is 5348 00> 0:1:58 Frequency is 90000 00> 0:1:58 The real number is 62429 00> 0:1:58 The imag number is 4744 00> 0:1:58 This is the start of the sweep function 00> 0:1:58 Frequency is 20000 00> 0:1:58 The real number is 6417 00> 0:1:58 The imag number is 61506 00> 0:1:58 Frequency is 25000 00> 0:1:58 The real number is 6798 00> 0:1:58 The imag number is 62907 00> 0:1:58 Frequency is 30000 00> 0:1:58 The real number is 6942 00> 0:1:58 The imag number is 64272 00> 0:1:58 Frequency is 35000 00> 0:1:58 The real number is 6875 00> 0:1:58 The imag number is 80 00> 0:1:58 Frequency is 40000 00> 0:1:58 The real number is 6588 00> 0:1:58 The imag number is 1348 00> 0:1:58 Frequency is 45000 00> 0:1:58 The real number is 6085 00> 0:1:58 The imag number is 2544 00> 0:1:58 Frequency is 50000 00> 0:1:58 The real number is 5332 00> 0:1:58 The imag number is 3603 00> 0:1:58 Frequency is 55000 00> 0:1:58 The real number is 4502 00> 0:1:58 The imag number is 4481 00> 0:1:58 Frequency is 60000 00> 0:1:58 The real number is 3478 00> 0:1:58 The imag number is 5170 00> 0:1:58 Frequency is 65000 00> 0:1:58 The real number is 2388 00> 0:1:58 The imag number is 5662 00> 0:1:58 Frequency is 70000 00> 0:1:58 The real number is 1212 00> 0:1:58 The imag number is 5925 00> 0:1:58 Frequency is 75000 00> 0:1:58 The real number is 49 00> 0:1:58 The imag number is 5951 00> 0:1:58 Frequency is 80000 00> 0:1:58 The real number is 64441 00> 0:1:58 The imag number is 5759 00> 0:1:58 Frequency is 85000 00> 0:1:58 The real number is 63373 00> 0:1:58 The imag number is 5348 00> 0:1:58 Frequency is 90000 00> 0:1:58 The real number is 62419 00> 0:1:58 The imag number is 4744 00> 0:1:58 This is the start of the sweep function 00> 0:1:58 Frequency is 20000 00> 0:1:58 The real number is 6416 00> 0:1:58 The imag number is 61508 00> 0:1:58 Frequency is 25000 00> 0:1:58 The real number is 6788 00> 0:1:58 The imag number is 62900 00> 0:1:58 Frequency is 30000 00> 0:1:58 The real number is 6951 00> 0:1:58 The imag number is 64283 00> 0:1:58 Frequency is 35000 00> 0:1:58 The real number is 6875 00> 0:1:58 The imag number is 84 00> 0:1:58 Frequency is 40000 00> 0:1:58 The real number is 6586 00> 0:1:58 The imag number is 1348 00> 0:1:58 Frequency is 45000 00> 0:1:58 The real number is 6083 00> 0:1:58 The imag number is 2544 00> 0:1:58 Frequency is 50000 00> 0:1:58 The real number is 5362 00> 0:1:58 The imag number is 3631 00> 0:1:58 Frequency is 55000 00> 0:1:58 The real number is 4512 00> 0:1:58 The imag number is 4477 00> 0:1:58 Frequency is 60000 00> 0:1:58 The real number is 3495 00> 0:1:58 The imag number is 5179 00> 0:1:58 Frequency is 65000 00> 0:1:58 The real number is 2388 00> 0:1:58 The imag number is 5669 00> 0:1:58 Frequency is 70000 00> 0:1:58 The real number is 1226 00> 0:1:58 The imag number is 5913 00> 0:1:58 Frequency is 75000 00> 0:1:58 The real number is 43 00> 0:1:58 The imag number is 5955 00> 0:1:58 Frequency is 80000 00> 0:1:58 The real number is 64427 00> 0:1:58 The imag number is 5760 00> 0:1:58 Frequency is 85000 00> 0:1:58 The real number is 63373 00> 0:1:58 The imag number is 5344 00> 0:1:58 Frequency is 90000 00> 0:1:58 The real number is 62425 00> 0:1:58 The imag number is 4740 00> 0:1:59 This is the start of the sweep function 00> 0:1:59 Frequency is 20000 00> 0:1:59 The real number is 6416 00> 0:1:59 The imag number is 61509 00> 0:1:59 Frequency is 25000 00> 0:1:59 The real number is 6788 00> 0:1:59 The imag number is 62902 00> 0:1:59 Frequency is 30000 00> 0:1:59 The real number is 6952 00> 0:1:59 The imag number is 64290 00> 0:1:59 Frequency is 35000 00> 0:1:59 The real number is 6876 00> 0:1:59 The imag number is 84 00> 0:1:59 Frequency is 40000 00> 0:1:59 The real number is 6580 00> 0:1:59 The imag number is 1367 00> 0:1:59 Frequency is 45000 00> 0:1:59 The real number is 6083 00> 0:1:59 The imag number is 2545 00> 0:1:59 Frequency is 50000 00> 0:1:59 The real number is 5348 00> 0:1:59 The imag number is 3616 00> 0:1:59 Frequency is 55000 00> 0:1:59 The real number is 4508 00> 0:1:59 The imag number is 4479 00> 0:1:59 Frequency is 60000 00> 0:1:59 The real number is 3476 00> 0:1:59 The imag number is 5169 00> 0:1:59 Frequency is 65000 00> 0:1:59 The real number is 2387 00> 0:1:59 The imag number is 5664 00> 0:1:59 Frequency is 70000 00> 0:1:59 The real number is 1230 00> 0:1:59 The imag number is 5922 00> 0:1:59 Frequency is 75000 00> 0:1:59 The real number is 45 00> 0:1:59 The imag number is 5950 00> 0:1:59 Frequency is 80000 00> 0:1:59 The real number is 64431 00> 0:1:59 The imag number is 5760 00> 0:1:59 Frequency is 85000 00> 0:1:59 The real number is 63373 00> 0:1:59 The imag number is 5345 00> 0:1:59 Frequency is 90000 00> 0:1:59 The real number is 62430 00> 0:1:59 The imag number is 4741 00> 0:1:59 This is the start of the sweep function 00> 0:1:59 Frequency is 20000 00> 0:1:59 The real number is 6415 00> 0:1:59 The imag number is 61510 00> 0:1:59 Frequency is 25000 00> 0:1:59 The real number is 6795 00> 0:1:59 The imag number is 62912 00> 0:1:59 Frequency is 30000 00> 0:1:59 The real number is 6946 00> 0:1:59 The imag number is 64275 00> 0:1:59 Frequency is 35000 00> 0:1:59 The real number is 6873 00> 0:1:59 The imag number is 82 00> 0:1:59 Frequency is 40000 00> 0:1:59 The real number is 6585 00> 0:1:59 The imag number is 1351 00> 0:1:59 Frequency is 45000 00> 0:1:59 The real number is 6079 00> 0:1:59 The imag number is 2537 00> 0:1:59 Frequency is 50000 00> 0:1:59 The real number is 5370 00> 0:1:59 The imag number is 3619 00> 0:1:59 Frequency is 55000 00> 0:1:59 The real number is 4507 00> 0:1:59 The imag number is 4479 00> 0:1:59 Frequency is 60000 00> 0:1:59 The real number is 3504 00> 0:1:59 The imag number is 5161 00> 0:1:59 Frequency is 65000 00> 0:1:59 The real number is 2383 00> 0:1:59 The imag number is 5662 00> 0:1:59 Frequency is 70000 00> 0:1:59 The real number is 1228 00> 0:1:59 The imag number is 5922 00> 0:1:59 Frequency is 75000 00> 0:1:59 The real number is 39 00> 0:1:59 The imag number is 5942 00> 0:1:59 Frequency is 80000 00> 0:1:59 The real number is 64436 00> 0:1:59 The imag number is 5759 00> 0:1:59 Frequency is 85000 00> 0:1:59 The real number is 63373 00> 0:1:59 The imag number is 5344 00> 0:1:59 Frequency is 90000 00> 0:1:59 The real number is 62431 00> 0:1:59 The imag number is 4731 00> 0:1:59 This is the start of the sweep function (Connection lost)
The data looks OK, except the values from the Re and Im registers have to be converted to decimals taking into account that the highest bit is the sign, so any reading above 32767 (hex 7FFF) is a negative value, so should be converted as reading = reading - 65536 (hex 10000).