Post Go back to editing

I need a reference circuit for 4_wire the impedance measurement using AD5934, range 50 to 250 ohm.

Thread Summary

The user asked for a 4-wire impedance measurement circuit for the AD5934, with an impedance range of 50 to 250 ohms. The final answer provided guidance on ensuring the signal amplitude at the ADC input is within the specified range and discussed the importance of the clock frequency and the DFT unit's accuracy. The user also encountered issues with the real and imaginary parts of the impedance measurements, which were addressed by converting the hex values to decimal and accounting for the sign bit. The user was informed that multiple AD5934 ICs cannot be used on a single I2C bus due to having the same address, and a TCA9545A I2C bus switch was suggested as a solution.
AI Generated Content
Category: Hardware
Product Number: AD5934

I saw the reference design file CN0349 and CN0217, I think both are 2-wire implementation of the AD5P3x family IC. Can I get the circuit reference for the 4-wire implementation, with impedance range of 50 to 250 ohm. 

Help will be highly appreciated. 

Parents Reply
  • Let me add the pictures of the waveform.

    100Ohm 

    120 ohm

    AD9534 frequency is 5khz and sweep increment I set to 4 Hz. The acquired signal amplitude does changes but I get 91 Ohm when I place 120 Ohm resistor after calibration.  

    After calibration with 100 ohm, when I do measure 100 ohm I get 100 ohm.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.