I saw the reference design file CN0349 and CN0217, I think both are 2-wire implementation of the AD5P3x family IC. Can I get the circuit reference for the 4-wire implementation, with impedance range of 50 to 250 ohm.
Help will be highly appreciated.
AD5934
Production
The AD5934 is a high precision impedance converter system
solution that combines an on-board frequency generator with a 12-bit, 250 kSPS, analog-to-digital...
Datasheet
AD5934 on Analog.com
I saw the reference design file CN0349 and CN0217, I think both are 2-wire implementation of the AD5P3x family IC. Can I get the circuit reference for the 4-wire implementation, with impedance range of 50 to 250 ohm.
Help will be highly appreciated.
You may use this post as a starting point:
In the link, it is mentioned that setting Rcal = 20 can set the impedance range from 1 to 60. Can you please explain this, I did not get this. How can Rcal resistor set the range.
For this part, I got the answer.
"The accuracy achieved is very much dependent on how large the unknown impedance range is relative to the calibration resistor, RCAL. Therefore, in this example, the unknown impedance of 10.3 Ω measured 10.13 Ω, an approximate 2% error. Choosing an RCAL closer to the unknown impedance achieves a more accurate measurement; that is, the smaller the unknown impedance range is centered on RCAL is the more accurate the measurement. Consequently, for large unknown impedance ranges, it is possible to switch in various RCAL resistors to break up the unknown impedance range using external switches. The RON error of the switch is removed by calibration during the RCAL gain factor calculation. Using a switch to select various RFB values can optimize the dynamic range of the signal seen by the ADC.
Consequently, for large unknown impedance ranges, it is possible to switch in various RCAL resistors to break up the unknown impedance range using external switches. The RON error of the switch is removed by calibration during the RCAL gain factor calculation. Using a switch to select various RFB values can optimize the dynamic range of the signal seen by the ADC. In addition, note that to achieve a wider range of measurements a 200 mV p-p range was used. If the unknown Z is a small range, a larger output voltage range can be used to optimize the ADC dynamic range."
Reference link below, page 3.
https://www.analog.com/media/en/reference-design-documentation/reference-designs/CN0217.pdf
How can Rcal resistor set the range.
Rcal does not set the range, it is used to measure the system gain, e.d. to find the dependence between the impedance under test and the output values produced in response. If you are planning to work with the circuit from the link you mentioned the factors setting the range are:
1. The excitation voltage programmed into the AD5933
2. Value of the current-setting resistor Rlimit
3. Gain of the instrumentation amplifier INAMP
4. PGA gain programmed into the AD5933
Choosing an RCAL closer to the unknown impedance achieves a more accurate measurement
This statement is correct only in case when the measurement accuracy does not depend on the value being measured. This is hardly the case with the circuit from the link you mentioned - the lower the impedance of the "BODY" - the lower the sinewave signal coming to the AD5933's internal ADC and the smaller the portion of the ADC's available dynamic range utilized in digitizing the signal leading to fewer digital steps approximating the sinewave, e.d. the higher discretization error. By using low values of Rcal for low expected values of the "BODY" impedance this higher discretization error is experienced twice: at the calibration stage and at the measurement one, so both the gain calibration and the measurement are not accurate. Also, the error acquired in calibration at low Rcal expands, when such calibration is used to calculate the unknown impedance of value higher than Rcal.
A better approach would be to choose the Rcal value so that the internal ADC would receive the sinewave spanning the majority of the ADC's available dynamic range (which would be about Vdd - 0.2V). In this case the accuracy of the calibrated gain would be close to the maximum achievable with the AD5933. Same is true with the unknown impedance: to achieve maximum available accuracy the signal coming to the AD5933 should be as close to the Vdd - 0.2V as practical, but should not exceed it. Therefore, in practice, with the circuit from your link, Rcal should be equal to the maximum expected value from the range. AS the unknown impedance getting lower the measurement accuracy is going to decrease, but one can either increase the excitation voltage, reduce the value of Rlimit, increase the gain of INAMP and/or program in PGA gain of 5 into the AD5933 or combination thereof, BUT making sure that the signal swing at the ADC input does not exceed Vdd - 0.2V. Exceeding it causes distortion of the sinewave, most often clipping at the power sully rails, the ADC mindlessly digitizes the distorted sinewave, which is fed to the "DFT," which does not know the sinewave is distorted and produces erroneous results without any warning to the user.
One more reiteration: the above is true for the 4-wire circuit from your link - it is the opposite when evaluation board or similar circuit is used. With the evaluation board Rcal should be equal the lowest impedance from the range to be measured.
Thanks for the detailed answer. The link was just a reference.
I am following this one,
https://www.instructables.com/Bio-Impedance-Analysis-BIA-With-the-AD5933/
But I need couple of small change, 1) my impedance range is from 50-250 Ohm, and 2) VDD is 3.3V. What changes should I do. I should just focus on the gain, (gain should be in the range of the internal ADC)?
If I use different power source for my MCU, can I use this design.
If yes, what changes you suggest for achieving my impedance range.
Thanks.
I also did simulation of the given design, does this design is fine or it needs any modification.

And the output waveform of U4 look like this.

gain should be in the range of the internal ADC)?
Yes, it is necessary to make sure that the circuit has gain that keeps the signal at the ADC input within 0.2V to Vdd - 0.2V for the entire expected range of the impedance to be measured.
The circuit you posted has 3 different sources of power: +4.096V, +12V and -12V - not sure which "different power source" you are asking about. Is your MCU is powered by 5V instead of 3.3V you mentioned earlier? You can certainly power the AD5933 and additional circuits with the same 5V with the caveat that digital circuits tend to produce high-frequency spikes on on their power lines that can somewhat reduce the measurement accuracy. You can always use some linear regulator to get improved 3.3V from the 5V MCU power supply. Also, this circuit is not a 4-wire impedance measurement.
R11 and R5 are connected in parallel to each other. If R5 seems to represent the impedance to be measured, then R11 has no function in this schematic and should be removed.
First thing to change would be to increase R3 to some reasonable value, say 1k for now, - it is the current-setting resistor for your impedance R5. When it is 0 - it instructs U2 to produce infinitely large current through R5, which requires infinite output voltage, which is impossible in practice, so U2 output slams into the power supply rails. When simulating, check that the output voltage of U2 is a well-formed sine wave of about 0.1V in amplitude
Second thing would be to remove R10 for now - the circuit does not need that much gain from INAMP. INAMP specs call for min 4.5V power supply voltage, so in your circuit at 3.3V Vdd it is operated out of spec. Perhaps it can still work, but will require some fiddling with the Input Common-Mode Voltage Range vs. Output Voltage, please see datasheet Fig 28, where it is specified for 5V Vdd. It is hard to predict how it is going to scale at 3.3V Vdd, maybe the model will be able to tell that. The desired behaviour would be for the OUTPUT VOLTAGE to have a baseline of Vdd/2 = 1.65V and to be able to swing from 0.2V to 3.1V undistorted. To achieve that it may be required to re-bias the U1 and U2 to lower voltage, perhaps somewhere down to 0.8V or lower to get into the INPUT COMMON-MODE VOLTAGE range, where there would be no signal distortion.
To summarize, lets increase R3 to 1k, remove R10 and run the simulation. U2 output should be a well-formed sine wave of 0.1V amplitude and DC bias of 1.65V. We would like to see the U4 output to be a well-formed sine wave of the same amplitude and bias, but likely it is not going to happen until U1 and U2 are rebiased to lower DC voltage - that would be the next step.
Please feel free to attach LT Spice models to your posts via Insert->Image/Video/File (you might need to zip the file if the system refuses).
P.S. You might want to consider using INAMP with lower power supply voltage requirements, usually referred to as "single-supply" INAMPS such as INA331, MAX4462, AD8223, etc.
Thanks for your time and for the great explanation.
I did some changes and I attached the Lt Spice file. Now, I am getting sinewave on the output.
Please, check the file, and waiting for your suggestions.
Thanks once again.2477.50-250-range.asc
Thanks for your time and for the great explanation.
I did some changes and I attached the Lt Spice file. Now, I am getting sinewave on the output.
Please, check the file, and waiting for your suggestions.
Thanks once again.2477.50-250-range.asc
Congrats, your simulation works! You have probably noticed that the model gets stuck, when the U4 output approaches certain amplitude (about 0.65V) when reducing R4 to give U4 larger gain - this is likely indication that signal hits the boundaries of that "box" on Fig, 28 in the AD8220 datasheet or rather the unknown boundaries of that "box" at the off-spec 3.3V power voltage.
Some general remarks regarding your model:
1. What does R12 represent? If this is the internal impedance of the AD5933 VOUT source, its value should be taken form Table 5. "Voltage Levels Respective Bias Levels for 3.3 V" on p. 13 of the AD5933 datasheet
2. What does R11 represent? It seems to have no function in this schematic and should be removed
3. What would be the function of C2 - it only reduces the signal and shifts its phase, perhaps should be removed
4. R8 and R9 are probably unnecessary, at least one of them or both should be removed
What would you want to do next? Tune this model to work with the AD5933? Try some different instrumentation amplifier? Some additional gain should be added to the AD5933 input OPAMP to obtain the amplitude of Vdd/2 - 0.2V = 1.45V for optimal use of the ADC input dynamic range.
Thank you for your comments.
I changed AD8229 To AD8227.
1. R12 is for the internal impedance of the IC, I just use 1k, but it depends on the range: AD593x has 4 different range. This I will remove from my schematic.
2. R11, I will add in my PCB just as a protection, I want to measure the tissue impedance. This resistor will have very large value (100-200 kOhms) compared to the tissue (approx 120 ohms) and for all normal operations this will not draw any noticeable current and the impedance of the parallel connection is dominated by the impedance of the tissue. If the impedance of the tissue should rise (e.g. pads coming loose) the current can then go through this resistor and the maxing out of the op-amp would not create unpleasant voltages on the pads.
3. C2 , tissue has capacitance, though the electrical model for the tissue is a little bit different, but this I just add for testing and this will not be the part of my PCB.
4. R8, R9, is for simulation, I add these to complete the circuit. This is not part of the PCB schematic.
Now I am designing my PCB, I will do the tuning, I can also use AD593x gain.
I changed AD8229 To AD8227.
1. R12
2. R11,
3. C2
It is common to use sequential RC to roughly approximate the tissue with electrodes, C models electrode-tissue interface, strongly depends on the nature and area of the electrode. Strictly speaking, it is C-R-C, but it is equivalent to R-C/2.
4. R8, R9
The model works without those two, just with a piece of wire connected to the INAMP output going nowhere, just for the probe to point at. But it is indeed a good practice to close the circuit and INAMP performance indeed depends on the load.
I changed AD8229 To AD8227
With the AD8227, without any rebiasing, the model indicates that the maximum amplitude AD8227 can output is about 0.55V, so the output sine wave swings between 1.1V and 2.2V. So to get the optimum signal at the AD5933 RFB pin (assuming the PGA gain is 1) it would be useful to get a gain of about 2.6 from the AD5933 internal OPAMP when your impedance to be measured is at the to of your expected range of 250 Ohm.
Minor point on the circuit - there is no need for two resistors R1 and R2 - can be replaced with one resistor running from the "+" of U1 to the output of U3. Please see 2477.50-250-range-1.asc with some edits attached.
Hope you are not rushing with PCB design, is this an educational project or a hobby?
Thanks for the simulation file, discussion with makes a lot of things clear to me.
PCB is not expensive in China, but, as you said I will not rush.
I want to make a Cardiac 3D mapping system (from scratch), currently I am working on impedance part. Whole system is a challenging task but not impossible. For now it is a hobby.
We (me and my friend) are also working on some other interesting stuff, if you want we can talk.
R8, R9
Yes, no need to use 2 resistors, I just use 2 resistors and it has no reason.
it would be useful to get a gain of about 2.6 from the AD5933 internal OPAMP
Yes, I was planning to do so.
Good luck with your project! Depending on the AD5933 frequency range and other settings programmed in you might bump into some unexpected/undocumented behavior, please do not hesitate to post your questions to this forum.
Thank you,
Do I need some filtering on the two input pins?
I have another question,
Do I need any sort of filtering in the receiver end, before any amplification.
Not sure if it is needed, does your application require galvanic decoupling of the impedance to be measured form the electronics?
It really depends on a particular use case - filtering is always tricky as it is not really known what to filter for unless the circuit is tested in real-life application and particular sources of interference are identified. The circuit itself in this 4-wire arrangement is reasonably resistant to environmental interference thanks to common-mode rejection. The high-frequency interference is likely to be sufficiently suppressed by relatively slow INAMP (250 KHz) and the AD5933 built-in 100 KHz low-pass filter.
What is the excitation frequency range you are planning to use? For impedance under test with capacitive response there might be a case for using an additional low-pass filter on the excitation side to filter out high-frequency spikes between the DAC steps in the synthesized voltage sine wave.