Post Go back to editing

synchronizing two dds to create quadrature dds

Thread Summary

The user asked if it's possible to generate a quadrature oscillation output (sine and cosine) using two AD9833 chips. The solution involves sharing the same MCLK and SPI, initializing one chip with a 90° phase shift, and asserting both CS lines simultaneously when writing the frequency word. The AD9106 was suggested as an alternative with a similar interface, but the user must use AD9833.
AI Generated Content
Category: Choose a category
Product Number: ad9833

Is it possible to create a quadrature oscillaion optput from two AD9833. I need changable quadrature signal, sine and cosine. What is the solution?

I have seen this:

Synchronizing Multiple AD9850/AD9851 DDS-Based Synthesizers Application Note (AN-587) (analog.com)

But AD9833 does not contain W_CLK and FQ_UD.

Edit Notes

new observation on synchronization appication note
[edited by: mohammadsdtmnd at 6:09 AM (GMT -4) on 25 Aug 2022]