Post Go back to editing

Problem for finding complete working code and connection of AD5934 IC with Arduino uno

Category: Hardware
Software Version: Arduino uno 1.8.2

I am trying to interface AD5934 IC with Arduino UNO ...I am not getting exact hardware connection and complete working of coding part.

I am trying to calculate impedance measurement and calibration part using AD5934 IC with Arduino UNO .

Please any one could help me out for this tissue.

I have a deadline of 1 week to complete this project.

I have tried in all possible ways.

Please could any one can help me out is more greatful to me.

Parents
  • I have tried in all possible ways

    What is the state of your project at this point besides its urgency? Do you have your Uno board connected to your PC? If so, can you load and execute any (AD5934 unrelated) demo sketch with it? If so, can you hook up your AD5934 chip (pinout is identical to the AD5933 shown) to your Uno according to the diagram:

     ?

    If you have done that, can you Copy/Paste the code form Antonius's AD5934-Arduino-Driver link into your environment, compile and execute it? If not, what would be the holdup?

  • Like this i have connected...

    This is AD5934 IC according to datasheet i have connected 

    Please do suggest me 

  • From your diagram and the picture it is not clear if you connected all supply pins to Vdd and all ground pins to GND, as recommended in the datasheet, p.8, Fig. 3:

    NOTES:
    1. IT IS RECOMMENDED TO TIE ALL SUPPLY CONNECTIONS (PIN 9, PIN 10, AND PIN 11)
    AND RUN FROM A SINGLE SUPPLY
    2. IT IS ALSO RECOMMENDED TO CONNECT ALL GROUND SIGNALS TOGETHER (PIN 12, PIN 13, AND PIN 14)

    Please check if all the pins mentioned connected accordingly.

    i just complied it

    So it sounds like the driver code from Antonius's post does compile without any errors. If you use a conventional Arduino environment you can print the valuers collected from the chip over serial port by adding to the code something like:

    1. Somewhere around line 179 -
    Serial.begin(9600);

    2. Somewhere around line 199 - 
    Serial.print(results.freq[cnt]);
    Serial.print(", ");
    Serial.print(results.realImp[cnt]);
    Serial.print(", ");
    Serial.println(results.imagImp[cnt]);

    Then upload your sketch and click Tools > Serial Monitor. 

Reply
  • From your diagram and the picture it is not clear if you connected all supply pins to Vdd and all ground pins to GND, as recommended in the datasheet, p.8, Fig. 3:

    NOTES:
    1. IT IS RECOMMENDED TO TIE ALL SUPPLY CONNECTIONS (PIN 9, PIN 10, AND PIN 11)
    AND RUN FROM A SINGLE SUPPLY
    2. IT IS ALSO RECOMMENDED TO CONNECT ALL GROUND SIGNALS TOGETHER (PIN 12, PIN 13, AND PIN 14)

    Please check if all the pins mentioned connected accordingly.

    i just complied it

    So it sounds like the driver code from Antonius's post does compile without any errors. If you use a conventional Arduino environment you can print the valuers collected from the chip over serial port by adding to the code something like:

    1. Somewhere around line 179 -
    Serial.begin(9600);

    2. Somewhere around line 199 - 
    Serial.print(results.freq[cnt]);
    Serial.print(", ");
    Serial.print(results.realImp[cnt]);
    Serial.print(", ");
    Serial.println(results.imagImp[cnt]);

    Then upload your sketch and click Tools > Serial Monitor. 

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.