Whether the AD9824 can generate a 10k square wave, the frequency jitter is preferably within ±1Hz. If not, can a square wave with frequency jitter within ±3Hz be generated.
KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
AD9834
Production
The AD9834 is a 75 MHz low power DDS device capable of producing high performance sine and triangular outputs. It also has an on-board comparator that...
Datasheet
AD9834 on Analog.com
AD9824
Not Recommended for New Designs
The AD9824 is a complete analog signal processor for CCD applications. It features a 30 MHz single-channel architecture designed to sample and condition...
Datasheet
AD9824 on Analog.com
Whether the AD9824 can generate a 10k square wave, the frequency jitter is preferably within ±1Hz. If not, can a square wave with frequency jitter within ±3Hz be generated.
I think you mean frequency resolution. The smallest frequency step is calculated as fMCLK/2^28.
Jitter depends on the stability of the MCLK clock source and the noise in the supply.