Post Go back to editing

AD9850 - seperate AVDD DVDD

Thread Summary

The user asked about the maximum voltage difference between AVDD and DVDD for the AD9850, and whether it's worth using separate supplies in a 30-88 MHz radio design. The final answer stated that AVDD and DVDD should be at the same potential, and using a single supply with ferrite bead isolation is a viable alternative. The AD9850 can output frequencies up to 62.5 MHz with a 125 MHz reference clock, and the user confirmed the actual DDS frequency range is 0.4 to 1.4 MHz.
AI Generated Content

What is the maximum voltage difference allowed between AVDD and DVDD with an AD9850?

I would like to use DVDD = 3.3V, AVDD = 5V.

Is there a list of which pins are referenced to AGND and which are referenced to DGND?

Final question - is it worth the effort to use seperate supplies? 

I'm using this in a 30-88MHz radio and the current design uses a single supply for the 9850.

Thanks

Randy

  • Hi, Randy!

    Different sources do not possible.

    Datasheet  AD9851 from:

    +Vs collectively refers to the positive voltages applied to DVDD, PVCC and AVDD. Voltages applied to these pins should be of the same potential

    AD9851 and AD9850 are as twin brothers,  and structure of sourcing is same.

    Regards!

  • Hi Randy,

    DVDD and AVDD should have the same supply. Kindly note that different specifications goes for 3.3V and 5V. Example:

    There is no specific list, you should just take note what circuitry each pin is associated. You may start reading at the pin function description.

    Yes, it is worth the effort to use separate supplies. However, this also comes with additional cost. You may use ferrite bead to isolate supplies as an alternative.

    Are you sure you are using AD9850 for frequencies 30-88MHz? AD9850 comes with a 125MHz reference clock so it can output frequency up to 1/2 the reference clock. That means, 30-62.5MHz is okay. above 62.5MHz up to 88MHz, you are using the aliased images of the DDS output. You may want to use other DDS with higher reference clock like AD9851 (180MHz ref clock).

    -Sitti

  • Thank you Sitti,

    You are correct on the frequency.  The DDS is a reference for a div 64 PLL so the DDS frequency is ~0.4 to 1.4MHz using a 10MHz clock.

    I'll end up using a single supply with ferrite isolation between the A & D supplies..

    Randy,