Post Go back to editing

Using SPI (from FPGA) to control AD9914 for single tone output

Thread Summary

The user is troubleshooting an issue with no output from the AD9914 DDS evaluation board when attempting to generate a single tone using an FPGA. The final answer indicates the thread is closed, suggesting the issue was resolved offline. Key clarifications include checking the jumper settings (P203, P204, P205) to ensure external control is properly configured, and ensuring all control pins, including profile pins, are not floating. The default profile when P205 is disabled is profile 7, which must be addressed for configuration.
AI Generated Content

Hi I have an evaluation card for the AD9914 DDS (AD9914/PCBZ) but wanted the FPGA to control the DDS to generate a simple single tone from one Profile registers. However I did not see any output after setting up the registers. Below are my sequence o commands

I set up the SPI sequence of the following:

1) Upon power up, issue Reset (Reset_Buf)

2) Write to register 0x03 to enable DAC Calibration (bit 24 = '1')

3) Write to register 0x03 again to clear DAC Cal (bit 24 ='0')

4) Write to register 0x01 to enable Profile Mode Enable

5) Write to register 0x0B to set up Profile 0 Frequency tuning word

6) Write to register 0x0C to set up Amplitude scale

7) Pulse IOUpdate

Does that sequence seem resonable or am I missing something?

Parents
  • Note, when the jumpers mentioned above are set to disable, the outputs of the ICs on the evaluation board driving the DDS are tri-stated. This to avoid BUS contention from external control. However, all the output nodes of these ICs then need to be tied off or controlled. It sounds like you're controlling reset and IO-UPDATE but other pins must be controlled too instead of floating. For example, down let the EXTPDCTL or SYNC_IO pins float. Also, the profile pins need to be configured to the internal profile register you're pointing to.

Reply
  • Note, when the jumpers mentioned above are set to disable, the outputs of the ICs on the evaluation board driving the DDS are tri-stated. This to avoid BUS contention from external control. However, all the output nodes of these ICs then need to be tied off or controlled. It sounds like you're controlling reset and IO-UPDATE but other pins must be controlled too instead of floating. For example, down let the EXTPDCTL or SYNC_IO pins float. Also, the profile pins need to be configured to the internal profile register you're pointing to.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.