Post Go back to editing

single clock oscillator for 16 AD5933  chips

Thread Summary

The user inquires about using a single 100kHz clock oscillator to supply 10 AD5933 chips. The engineer confirms it is possible with a clock buffer like the LMK00101 from Texas Instruments, and advises against using the LTC6906 due to high jitter. A 100kHz crystal oscillator is recommended for direct connection to the clock buffer.
AI Generated Content

Hello I am using 16 AD5933’s with a clock frequency of 10kHz. I want to know whether i can use single clock oscillator to supply for 16 chips (OR) 16 clock oscillators to supply to 16 AD5933 chips.