Post Go back to editing

AD9914, AD9959 Eval Software Dev API

Thread Summary

The user seeks an SDK or the source code of the AD9914/AD9959 evaluation board GUI to interface with the boards via USB using custom software. The support engineer provided Python code for the AD9914 but noted that no such code exists for the AD9959. The user requested any available code, regardless of language.
AI Generated Content

I'd like to be able to interface with the AD9914 amd AD9959 evaluation boards via USB using my own software (written either in C++ or python). This is similar to other posts - see:

Re: AD5370 Eval - Software Development API - CYPRESS USB (EZUSB CYUSB)

AD5370, AD5371, AD5372 and AD5373 evaluation board software commands

Is there an SDK available for talking to the eval board over USB? If not, is the AD9914 / AD9959 GUI source code available for me to modify for my own purposes?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.