Post Go back to editing

AD9915 Spurious Output Question

Thread Summary

The user is experiencing unexpected spurs at 947.5 MHz (-71 dBc) and 942.5 MHz (-70 dBc) when using the AD9915 evaluation board with a 2.5 GHz SYSCLK. The Analog Devices support team did not observe these spurs in their setup and suggested checking the signal purity of the clock and power sources. The user confirmed that changing the clock sources and power supplies did not resolve the issue and requested spectrum snapshots with a wider span (50 or 100 MHz) to better diagnose the problem. The final answer indicates that the thread is closed, and the user is advised to post a new question if further assistance is needed.
AI Generated Content

I am using the AD9915 evaluation board with SYSCLK = 2.5 GHz and I am finding spurious content that is not predicted by the ADIsimDDS tool.  Two specific examples are for fOUT set at 927.5 MHz there is a spur at 947.5 MHz at -71 dBc and for fOUT set at 932.5 MHz there is a spur at 942.5 MHz at -70 dBc.  There are many other instances such as these and they are well below the cut-off of my reconstruction filter.  Are these spurs expected to be there or is there something wrong with my evaluation board or how I'm using it?  Can anything be done to reduce or eliminate these spurs?  Any help in this matter is greatly appreciated.

Parents
  • Hi Alan,

    We did a verification regarding your setup and the attached files contain the spectrum of it. However we do not see any spurs that you are seeing. Kindly check the signal purity of your clock and power sources, it might be the spurs were created due to the spurs which are present on those sources.

    Best Regards

    Louijie

Reply
  • Hi Alan,

    We did a verification regarding your setup and the attached files contain the spectrum of it. However we do not see any spurs that you are seeing. Kindly check the signal purity of your clock and power sources, it might be the spurs were created due to the spurs which are present on those sources.

    Best Regards

    Louijie

Children
No Data