Post Go back to editing

AD9959 Understanding and Accounting for Power Loss with Frequency

Thread Summary

The user is experiencing frequency-dependent power variation in a signal generator built with an AD9959 and Arduino Due. The final answer explains that this is due to the zero-order hold effect of the DAC, resulting in a sinc response, and suggests measuring the frequency response to apply amplitude correction. The AD9910 is recommended as a potential alternative with better amplitude ramping capabilities.
AI Generated Content

Hello all,

I apologize if this is the wrong place to ask things like this.

I've got more of theory based question today (I'm relatively new to signal processing/etc).

As this is the case I'm happy with just being told what sort of things I should research - the main issue seems to be that I don't know what I don't know.

For context, for the past month or so I've been building a signal generator using an AD9959 and an arduino due.

The purpose of this build was to get 3 channels outputting simultaneously, 1 channel having a constant frequency and the other 2 channels both doing independent frequency sweeps and amplitude ramps - this I have managed to do. The latter was achieved by using a for loop to assign amplitude values to the registers - this was done due to the limitations of the inbuilt amplitude ramping of the DDS, namely with a 500MHz the slowest I could get the ramp intervals was 2.048 us, an order of magnitude too fast for my purpose.

Now, an issue that I have been aware of for a while is that I get a variation in power with frequency - attached is a graph of some data illustrating this (I have set the power output to 'max' in the ACR register for each frequency).

My frequency range of interest is from ~20-110MHz.

My colleagues do not believe that my cables/wiring are the main reason this is happening, rather they suspect it has something to do with how the DDS works.

I do have a rough understanding of why the power drops with an increasing frequency. The system clock is sampled in a sense, i.e. with a 500MHz, at 125MHz the output would be generated from only the peaks/troughs and 'zero's' of the clock sine wave (i.e. 0, 1, 0, -1, 0). With a desired output being 250MHz, exactly half of 500MHz, the clock would be sample at only the 'zero's' of its sine wave, hence why I get no signal at 250MHz.

If my understanding is incorrect or id I'm just spouting nonsense then I'd appreciate it if I could be corrected! (I have read through the data sheet and All About Direct Digital Synthesis | Analog Devices ).

However can not wrap my head around is why I am getting the peak at ~20MHz and why I get a sharp drop off at 170MHz - what mechanisms could be behind this?

Any suggestions/explanations or pointers on topics to research would be greatly appreciated - I have an idea of a way I could correct for this in my code but I would very much like to actually understand why this is happening to begin with.

Now, the way I'm planning on correcting for this is by determining a power vs frequency function and correcting the amplitude/scaling in my for loop (syncing the timing of my AM for loop to the frequency sweep RDW and LSRR registers).

When I mean correcting I mean that inputting "100% amplitude" would give the same power regardless of frequency. Say with my range of 20MHz to 110MHz, then inputting "100% amplitude" to my device would give an output of -13.2 dBm (the max value at 110MHz) regardless of the frequency setting (provided less than 110MHz).

The issue with this would be that my amplitude resolution would be decreased at lower frequencies (for example, in order to get -13.2 dBm I'd need to send say "60% power" to the ACR register when the frequency is set to 20MHz).

Any suggestions on a better way to tackle this would be appreciated, as I find my proposed solution to be a bit crude.

Thank you for taking the time to read my wall of text, any and all advice/suggestions are greatly appreciated.

Cheers,

Chris.

attachments.zip
  • A fundamental loss of power with frequency is a consequence of the sample & hold nature of the DAC (the final output of the DDS). That is, at each sampling instant, the DAC outputs a DC level and holds that level until the next sample. This is a sampling characteristic known as zero-order hold and results in a predictable drop off in signal level with frequency. Namely, the familiar (or maybe not) sinc response:

    sinc(x)=[sin(pi*x)]/(pi*x)      <==  x is the ratio of the output frequency to the sampling frequency (f/Fs).

    Note, for f=0 (DC), we have sinc(0)=1, or 0dB. For f=250MHz and a 500MHz sample rate, we have sinc(1/2) = -3.92dB. For frequencies between DC and 250MHz, the output level follows the decreasing curve of the sinc function. Interestingly, some of our DDS devices have a built in digital filter that automatically compensates for the sinc roll off (unfortunately, the AD9959 is not one of them).

    Your output plot appears to follow the general feature of the sinc response. However, other factors can alter the frequency response and even swamp out the sinc response. For example, if you are using a transformer at the output, then it's frequency response plays a roll. Assuming you have a reconstruction filter at the output, its frequency response is a factor, as well. Then there are board traces, cabling, the phase of the moon, etc.

    In any case, your proposed method of amplitude correction sounds quite reasonable. If you measure the frequency response, then you can compensate via amplitude adjustment based on frequency.

  • Hey Kenny,

    Cheers for the reply, it is very much appreciated!

    I'm curious however, what are the DDS's that correct for the sinc response?

    A bit off topic:

    The AD9959 was just what we had on hand (and had the desired frequency ranges) and hence why I am using it to build a prototype.

    However, if I find another DDS which is better suited to my purposes (ramping amplitude from 0-100% in 10's of ms while being able to do a frequency sweep to a similar quality/time scale as the AD9959 - and doing these over multiple channels independantly) then I'd likely swap to that.

    One of the main limiting factors I've found with the AD9959 is that it was not built to natively carry out the types of "slow" (relative to what the AD9959 can do at a 500MHz sys clock) amplitude ramps I'm interested in. As a result, the amplitude scaling in the ACR register only has 10 bits of resolution.

    In any case, once again, thank you for all your help - on this question and on my previous ones.

    Cheers,

    Chris.  

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.