Post Go back to editing

About the output of AD9951

Thread Summary

The user encountered an issue with the AD9551 output filter where signals below 30 kHz were heavily attenuated due to the ADTT1-1+ balun's frequency response. The solution was to replace the ADTT1-1+ with the ADTT1-6+ balun, which operates better at lower frequencies. An alternative suggestion was to omit the transformer and couple directly to one side of the DAC, but this results in half the output voltage and a DC return to 1.8V.
AI Generated Content

Dear Forum

   I refer the official manual to design AD9551 ,and my output filter is refer AN-837 as follow,

 now my problem is when my output frequency is 100KHZ,it output normally,but when my output frequency below 30KHZ,it  hadn't output,the signal

at primary is 1.75V(DC),and the signal at secondary is zero,my balun is ADTT1-1+,I want to know why?

Parents Reply
  • NOte that the low frequency transformers are no good at VHF. If you do really need both high and low frequencies, then you can omit the transformer and just couple direct to one side of the DAC.  (put a dummy load resistor on the other side, dont leave it unconnected )

    However, then you only get half the voltage, and the load has it's DC return to 1.8V not to ground.

Children
No Data