Q.
Are there any specific recommendations regarding via fill material in the circuit board for the thermally enhanced package styles associated with some ADI DDSs?
-------------------
A.
The…
Q: Can I use DDS to produce modulation?
A: By default, DDS supports frequency modulation (FM), because the user can change the frequency tuning word on demand. DDS devices that allow user access to phase…
Frequently we're asked for help selecting a DDS with frequency sweeping capability, phase hopping, amplitude control etc. but until now the only way to answer that question was to go based on memory or…
This Direct Digital Synthesis tutorial with audio provides a description of the three fundamental elements of a direct digital synthesizer (DDS). Use the play button to start the presentation and advance…
This Direct Digital Synthesis tutorial with audio describes correcting for the DAC's sin(x)/x (or sinc) response. Use the play button to start the presentation and advance to the next slide. For more instructions…
This Direct Digital Synthesis tutorial with audio describes the function of the accumulator, the first DDS element. Use the play button to start the presentation and advance to the next slide. For more…
This Direct Digital Synthesis tutorial with audio describes the function of the angle-to-amplitude converter, the second DDS element. Use the play button to start the presentation and advance to the next…
This Direct Digital Synthesis tutorial with audio describes the function of the analog-to-digital converter (DAC), the third DDS element. Use the play button to start the presentation and advance to the…
This Direct Digital Synthesis tutorial with audio describes the function of the DAC reconstruction filter and provides a description of four types of analog filters. Use the play button to start the presentation…