Q
AD9915 can be used with directly 2500 MHz clock or 2500 MHz system clock which can be obtained from 100 MHz external clock with multiplier via PLL enabled. Which situation is useful for best performance…
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the