Article Is it possible to achieve a higher sampling rate from the MAX31855

No, the typical conversion time is 70ms, thus the sampling rate would be approximately 14 samples per second. The maximum conversion time is 100ms, thus the sampling rate would be 10 samples per second. You may read from the registers at a faster rate, since SPI serial-clock frequency is 5MHz (max), however the fault and temperature data are only updated once per conversion cycle, when /CS is high.    

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.