Article Multiplexing multiple thermocouples using MAX31855?

Providing that you do not ground any of those T- wires, it is possible to bundle them together at T- pin.   However, care must be taken regarding the RON resistance of the mux or switch, as a high RON will affect the voltage drop sensed across the T+/T- terminals for the active cable. 

While it is possible to bundle the T- connections, it is recommended to use a two input mux to separate each thermocouple channel in case noise is picked up by one of the cables, as that noise will affect all channels if the T- are connected together.

Wait two full conversion cycles (~200ms Max.) after you change your MUX before reading sensor.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.