Article Can ADN4604 do single ended 75Ohm input and output?

Question

The ADN4604 device looks like it can be configured in single ended mode. Can it
do single ended 75Ohm input and output?

Answer

The ADN4604 has internal 50-ohm termination single-ended resistors and is not
ideally suited to interface to 75-ohm transmission interfaces.

However if the application is for SDI video: SDI uses 75ohm single-ended
Coaxial Cables. In a typical application an SDI cable equalizer is used to
equalize the cable as well as convert from 75-ohm single-ended to 100 ohm
differential signalling, which is optimal for the crosspoint switch.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.