Article What three phase systems are supported by the ADE7912/ADE7913 or ADE7932/ADE7933?

Question

What three phase systems are supported by the ADE7912/ADE7913 or
ADE7932/ADE7933?

Answer

The isolation technology used inside the ADE7912/ADE7913 or ADE7932/ADE7933
guarantees that for 50 years lifetime, the three phase systems must have
maximum 400V rms values. This means three phase wye (3 phase 4 wires) and delta
(3 phase 3 wires) systems with nominal voltages of 230 Vrms are supported.
Delta systems with nominal voltages of 400 V rms are not supported as the
maximum voltages of these systems go above the 400 V rms limit.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.