Article AD7147: Can I use it to detect the hand at 10cm away from the button?

Question

Is it possible to use the AD7147 for an approximation, I want to
detect the hand at 10cm away from the button?

Answer

The proximity detection range for AD7147 is up to 2cm. Getting a detection
distance of 10cm is not possible with the cap touch parts AD7147/8. We have
other parts which offer more proximity distance range, AD7150/1 have 1 or 2
channels which can be dedicated to implement proximity detection with a range
of up to 5cm.
The range of the AD7150 is dependent on the actual sensor design/size/shape so
it may be possible to extend the range with large sensor.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.