Article AD5259 - "Not Connected Option - third logical stage "1", "0", "NC" ??

Question

in the Rev 0. of the AD5259 datasheet there is a table showing the possibility
to address 9 devices.

On stage is called "NC"


meaning I have A0 and A1

and the ligic Levels "1", "0" and "NC"

this allows to address 9 parts.

Where is this gone?


Answer

Analog Devices removed the "NC" option moving from datasheet Rev 0 to Rev A.

The part includes a current detector in these pins for the floating condition
(NC)
This circuit somehow is quite sensitive and it could fail under some
circumstances.

(In fact, some of the new digipots include this circuit but a malfunction is
detected at low voltage (

In order to avoid customer problems, these options were deleted from the DS.

The circuit is still inside the circuit so if you never experience problems
using these address (NC), he/she can continue using it but as these address are
not in the DS we cannot assume any responsibility and we are not able to
guarantee to function under all circumstances.


the normal way is:

The A0 and A1 are two state the Logic levels are specified

DIGITAL INPUTS AND OUTPUTS
Input Logic High VIH 0.7 × VL VL + 0.5 V
Input Logic Low VIL ?0.5 0.3 × VL V

With A0 and A1 - 4 parts are addressable by logic.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.