Article AD5235: Programming

Question

The problem is very simple. The seriel programming Signals are provided by the
FPGA, but the AD5235 doesnA?t store the value. I think I am not providing all
needed signals or timings. Is it possible to get an explanation how to connect
the chip, focus on CS, WP and PR?

Answer

If you are not using WR and PR, then you should tie them high.

The /PR pin is a digital input, applying a logic low, will refresh the contents
of the scatch pad memory (RDAC register) with the current contents of the EEMEM
memory.

At power-on, the default value of the scatch pad memory is the value previously
saved in the EEMEM, therefore, to answer your question, on power-on the value
of the scatch pad will be loaded with the previously loaded contents of EEMEM,
without applying a logic low to /PR, you don't need an RC circuit connected to
/PR to ensure that the scatch pad is refreshed, as this is automatic on
power-up.

To write to the part, you need only to connect CS, SDI and SCLK.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.