Article Does MAX9378 work with single-ended input?

Does MAX9378 work with single-ended input?

There should be no problem using MAX9378 with a single-ended input. However, one important thing to note is that the the output is indeterminate when the differential input voltage (|VID|) is less than 0.1V, per the differential input threshold specification on page 2 of the datasheet (Rev 1, 7/03).  Driving IN (pin 2) as a single ended input, for example, when /IN(pin3) is biased to 1.0 V, the output is indeterminate for IN (pin 2) voltage between 0.9V and 1.1V.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.