The MAX31856 is calibrated at the factory, and does not require any calibration. On page 4 of the MAX31856 datasheet, the Thermocouple Linearization Correction Error in °C can be found. Since the MAX31856…
Set bit7 (CMODE) of the CR0 (Configuration 0) register to 0 to set MAX31856 to standby mode. In this mode, the device will perform conversions only when bit 6 of Configuration 0 (the 1SHOT bit) is written…
If the internal temperature sensor is used for cold junction compensation, MAX31856 will assume that the device temperature and cold junction temperature are the same. When the connection is made in the…
It is not advised to use a grounded thermocouple with MAX31856. We do not intend the MAX31856 or any of Maxim's thermocouple ICs to be used with a grounded tip. The common mode voltage for the input is…
There are 2 situations that could lead to this issue:
1. Soldering: please check if soldering was done properly.
2. Radiation noise within the space: since the input is high impedance when the part…
MAX31856 needs to perform one conversion for the cold junction temperature and another conversion for thermocouple temperature to get a temperature reading. The fastest conversion occurs in the auto conversion…
The actual cold junction is where the thermocouple wires make first contact with a board, connector or plug (two dissimilar metals). The MAX31856 uses the internal die temperature of the IC to act as the…
If implementing a thermocouple near a high voltage bus, or in any environment with high EMI or RF noise, then the MAX31856 is recommended. The MAX31856 has on-board noise filtering, but also over/under…
Please read the cold junction temperature registers (0Ah and 0Bh) and check whether the linearized thermocouple temperature reading is fluctuating with the cold junction temperature. In the Electrical…