No, the MAX31855’s SPI interface must not have voltage higher than 4.0V applied. High voltage and high current (through a voltage-divider) will induce self-heat resulting in cold-junction and thermocouple…
No. The MAX31855 does not have any on-board 50/60Hz notch filtering, nor does it have any high frequency filters. A 10nF ceramic capacitor (maximum value) should be placed as close to theMAX31855 package…
No. While the MAX31855 does perform automatic cold-junction compensation, it does not perform any linearization calculations. Linearizing the thermocouple results needs to be performed externally using…
Yes, but you will lose some fault detection capability since you are intentionally grounding the T- portion of the cable, and you may experience a slight decrease in thermocouple temperature accuracy since…
Yes, when /CS is inactive high, the SDO (data out) pin is high-impedance (tri-stated). The MAX31855 will not drive a signal on the SDO pin when the chip select pin is inactive, and thus will not load the…
No, it is necessary to ensure that each MAX31855 is independently measuring the corresponding channel's thermocouple, with each thermocouple being independent. The T- cannot be connected. During the conversion…
There are two possible causes of this problem: 1. SPI communication error. If the reference junction temperature is confirmed to be at 35 degree, the reference junction reading is correct. If the temperature…
When using a signal generator or thermocouple simulator, it is recommended to connect directly to the T+ and T- of the MAX31855K. Long cable connections to the T+ and T- terminals of the MAX31855K may…
When a thermocouple's leads are connected in reverse to the MAX31855 T+/T- pins, you will see the reported value of thermocouple temperature decrease as the actual temperature at the thermocouple tip increases…