ADT7320: FAQ

  • Created
  • Updated
Was this helpful?
  • ADT7320, ADT7420

    Question Does the ADT7X20 need to be calibrated? Answer No user calibration is required with these sensors because ADI pre-calibrates all devices using our high accuracy test solution. Because each…
  • ADT7320, ADT7420 - Communication with ADT7x20

    Question How do I communicate with the ADT7320 and ADT7420? Answer The ADT7320 has a SPI 4-wire interface and the ADT7420 has an I²C 2-wire interface. The sensors will typically complete a conversion…
  • ADT7320, ADT7420 - Requirements to setup the ADT7320/ADT7420

    Question What additional components do I require to setup the ADT7320/ADT7420? Answer Both parts require a 0.1uf ceramic and 10uf tantalum decoupling capacitors. The interrupt and critical limit pins…
  • ADT7320, ADT7420 - Temperatur reading optiions

    Question Why do I have an option between 13 and 16 bit temperature readings? Answer In 16-bit mode the user has a resolution of 0.0078°C but in 13-bit mode the resolution is only 0.0625°C. However in…
  • What is the lifetime of the ADT7320?

    Question What is the lifetime of the ADT7320? (Stauts of 08_2013) Answer We guarantee the ADT7320 with a lifetime of at least 10 years, provided it operates according to the specifications outlined in…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.