AD8152: FAQ

  • Created
  • Updated
Was this helpful?
  • AD8152 EVB

    Question AD8152 EVB schematic Answer Please refer to the attached
  • AD8152: Connection of DC inputs

    Question I am running the AD8152 on VEE=0, VCC=+2.5V and would like to drive the inputs of the inputs, DC couple, from LVPECL with a common mode range of +1.5V to +2.3V. Can I connect VTTI to ground…
  • AD8152: used as a DVI switch

    Question Can you suggest whether AD8152 can be used in DVI application for the TMDS link switching? Answer We have not tested this, but everything should be good for the AD8152 to handle the TMDS signals…
  • AD8152_switch HDMI signals

    Question I want to use AD8152 as a HDMI cross point switch. Can I use the HDMI signal. Also if it can be used, can I cascade several AD8152s to implement a larger matrix. Answer 1. Yes, the AD8152…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.