AD7740: FAQ

  • Created
  • Updated
Was this helpful?
  • AD7740 AD7740: maximum input frequency

    Question I can't find the parameter about the maximum frequency of the input signal at the VIN Pin. Would you please give me some advices? Answer The 7740 uses a sigma-delta type architecture. The input…
  • AD7740_master clock frequency

    Question Question about AD7740 master clock frequencyVDD is 5V, REFIN is 5V, the crystal's frequency is 100kHz, BUF is connected to GND. Below is the test resultVin(V) 0 1.5 1.8 2 2.3 2.5 2.6 2.7 2.8 2…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.