AD5292BRUZ-50: FAQ

  • Created
Was this helpful?
  • AD5292 and extending SPI bus length

    Question I am using the AD5292, accessed via SPI. However, there is need to extend theSPI-bus to a length of 2,5m. Sadly, the AD5292 doesnt recognize sent bitscorrectly most of the times. I would be grateful…
  • AD5292: SPI Mode issues

    Question The problem is: The Pot does NOT work, when the SCK line is held high during idle. It needs to be held LOW! The datasheet (fig. 3 and 4) suggest, that it can be either high or low, which is…
  • AD5292BRUZ-50 SDO readback issue and power-up sequence

    Question/Issues AD5292BRUZ-50 SDO readback , power-up sequencing and operation stability issues. Answers To resolve AD5292BRUZ-50 SDO readback issue and the power-up sequence for Robustness and stability…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.