AD5259: FAQ

  • Created
  • Updated
Was this helpful?
  • AD5259 - "Not Connected Option - third logical stage "1", "0", "NC" ??

    Question in the Rev 0. of the AD5259 datasheet there is a table showing the possibility to address 9 devices. On stage is called "NC" meaning I have A0 and A1 and the ligic Levels "1",…
  • AD5259 I2C Device Address

    Question I would like to ask you about the I2C device address of AD5259. According to the documentation the complete address is changing by pins AD1 and AD0. In case of other components of the AD525x…
  • Decoding the tolerance register of AD5259

    Question Dear Sirs, using the AD5259 digital potentiometer, I want to make sure, I use the contentsof the tolerance registers correctly if the sign bit is set. How are negative values in the tolerance…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.