Question Is it possible to operate two AD2S1210 converters with one resolver?
Answer It is possible to operate two AD2S1210 covnerters with one resolver however
proper synchronisation procedure must…
Question The minimum excitation frequency of the AD2S1200 is 10kHz according to the data
sheet. Is there a mode
that the AD2S1200 can run with 2kHz excitation? Or is there an alternative part
that…
Question Do I need a separate 96 way connector cable to connect the EVAL-AD2S1210 board
to CED1Z board? And if yes, is it included in the CED1Z evaluation kit? Answer No cable is required. The EVAL-AD2S1210…
Question Is it possible to use the AD12S1210 as an interface for LVDTs?
Answer You can use the AD2S1210 to interface with an LVDT, but some extra
design is required in mapping the output from…
Question Can the AD2S1210 be operated with an externally generated sine wave reference? Answer It is tricky to synchronize the AD2S1210 to an external excitation.
To achieve it you must ensure that…
Question I have some doubts for the datasheet of AD2S1210:Q1:In the spec of AD2S1210, we can see the RDC system response block diagram in Page 32. There are five parameters:K1,K2,a,b and c. (Figure 1)They…
Question EXC/EXC- waveforms are correct when resolver is disconnected, but have some
distortion once we connect the resolver. What do think could be the cause of
this distorsion? Answer From your schematic…
Question My AD2S1210 customer always get Sin/Cos inputs clipping error even after
lowering the gain of the EXC's buffer circuit.
He also sees noise on Sin/Cos input and he would like to add a differential…
Question 1. One customer used TS2620N21E11+AD2S1210, and the resolver's parameter is below. if the resolver's input signal is 7Vrms, then SIN and COS input ofAD2S1210 will be bigger than the limitations…
Question My application uses two AD2S1210 (NUM 1 and NUM 2) simultaneously to decode two rotary resolvers. I am required to use only one AD2S1210 (NUM1) tooutput EXC signals to simultaneously drive two…