Post Go back to editing

CN0532 long term operating temperature

Thread Summary

The user inquired about the suitability of the CN0532 for monitoring vibration on equipment with surface temperatures of 90 to 110°C during 10-hour shifts, 6 days a week. The support engineer confirmed that all CN0532 components are rated to 125°C, but long-term reliability at high temperatures is not characterized. The ADXL1002 accelerometer may experience offset drift due to package degradation, potentially a few 100 mg over its lifetime, though this is application-dependent.
AI Generated Content
Category: Hardware
Product Number: CN0532

Hi, 

One of the equipment for which we want to monitor vibration has a surface temperature of 90 to 110 degree Celsius. These conditions are during 10 hour shifts, 6 days a week.
Is the CN0532 capable for the job? The datasheet says maximum operating temperature 125 degrees, but it doesn't say anything about long term reliability at high temperatures.

Regards,

  • Hi, 

    All CN0532 components are rated to 125C, but we did not characterize long term reliability of this circuit. Notice that the ADXL1002 (accelerometer on the CN0532) is on a over molded package, so package degradation/aging is expected at high temperatures. This would be translated as an offset drift at the output of the ADXL1002. Generally, we would expect the ADXL1002 to drift a few 100 mg over life time, but this is very difficult to quantify as is application dependent. 

    I hope this helps, 

    Pablo .

  • Hi Pablo,

    On your reply above, did you mean 100 mVDC or mg?  I am trying to quantify what kind of drift to expect on the DC offset due to this package degradation/aging.

    Thanks,

    LdlT

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.