I was wondering if somebody could provide some explanation as to what this error is and how to fix it, occurring with the Voyager 3, Condition Based Monitoring Platform. I was evaluating this system and it has been working fine for just under three weeks but out of nowhere I was not able to detect any mote due to this issue. I then reflashed the mote I was using and everything started working again but only for 15 minutes until the same error occurred. This is the only device similar to this we have in the office so I'm sure there is no interference occurring. The mote and gateway are with 30 cm of each other and it was working perfectly and stopped out of nowhere. Any help would be greatly appreciated, thanks.