Skip navigation
Log in to follow, share, and participate in this community.

Recent Activity

Andrew.Choi
Hi all   One of my customers uses the ADuCM330 in slave mode, she wants to communicate under certain circumstances without any request from master.   Initial state : Master sleep / Slave(ADuCM330) sleep The slave periodically checks the battery voltage and enters sleep mode again if it is normal. if the battery voltage is below the reference… (Show more)
in Other ADI Processors
RadioFrank
I have been working for a long time with ADSP-2187N in 144-BGA package (ADSP-2187NBCA-320) giving it as input clock a 40MHz sine wave (3Vpp) without any problem. Datasheet doesn't specify other characteristics. For obsolescence of BGA, I have switched to a 100-Lead LQFP (ADSP-2187NBSTZ-320). Now I'm finding some strange behaviours like not… (Show more)
in Other ADI Processors
ferario
I need to replace obsolete ADSP-2115 family with a new one hopefully code compatible. Is the ADSP-218xN family a good choice?
in Other ADI Processors
santhanakrishnan
.   I am using 2 ADSP TS201S Processors in my board. I am facing one issue with the link port communication. The link port communication (Only L2) is not happening in ambient temperature. Above 40 to 45°C this communication is happening. I dont know why it is behaving like this. During debugging process we have found the following things.   As i… (Show more)
in Other ADI Processors
digitalhcj
For ADSP-TS101S, it seems cclk is not stable and sometimes the chip fail to start. I doubt about the poor power design leading to unstable internal clock. I want to have a way to monitor internal clock directly.
in Other ADI Processors
g.amarnath17@gmail.com
Hello,   Since this part ADSP-TS201SABPZ060 is obsolete I couldn't find a pricing for the Chip.   Can you please help me by sending me an Quotation.   Qty - 1 No. 
in Other ADI Processors
rbedinfr
Hello, I am currently studying a bit of the TS-201S processor and I need to understand some of its conventions, such as parameter passing and stack frame construction. When doing the same for other processor brands, I usually looked for the processor programming manual and its "EABI" document, but I was not able to find such a document for the… (Show more)
in Other ADI Processors
lmirkin
Hello,   After using the ADSP-2191M for 15+ years we're looking for a new processor, mostly because VisualDSP++ 3.5 is not supported on current operating systems.   We're interested in a more recent processor that supports fixed-point arithmetic, has same/similar peripheral interfaces as the 2191, and would make migration relatively easy.   Are… (Show more)
in Other ADI Processors
kgk123
We designed a board using TS101S processor at 300MHz. Schematics taken from EZ-KitLite. The card is up and fine. JTAG scan passes and enters the Emulator Session via USB-ICE without any issue. We have not yet written anything in the boot flash, so the boot flash is blank. After power on, the first thing we do is, enter via USB-ICE emulator and… (Show more)
in Other ADI Processors
Andrew.Choi
Hi all   When the 11th bit (UARTMODE) of the LIN Interrupt Mask Register is enabled, is LIN communication (D / L) normally enabled by the 28th LIN I / O pin?   Thank you
in Other ADI Processors
Load more items