Skip navigation
Log in to follow, share, and participate in this community.

Recent Activity

omaryang
Is there any chip similar to AD5447 (high update rate)but with higher resolution like 16 bits
in Precision DACs
hiro@els
Hi all,   Our users will use the AD5767. They use the Dither function. Please let me know the input impedance value of the dither signal pin (N0,N1).   If you have a question, please let me know.   Best regards, Hiro
in Precision DACs
@Linear
How to deal with EXPOSED PAD of LTC7106? no remark in datasheet. Thank you very much.
in Precision DACs
pqpaul
Hi all,   how long I have to wait before writing the next command to the AD5671R?   Kind regards, Paul
in Precision DACs
gkasprow
I designed low noise 32-channel DAC modules for ion-trap applications. And we observe that on some of the boards the DAC consumes much higher current on negative rail than specified. I measure 60mA, this current heats the chip significantly and gets increased with every degree. At certain moment, the DAC and LDO gets hot and the LDO enters… (Show more)
in Precision DACs
ICHIBAN
We have a EVAL-AD5766 (both LFSP and WLCSP packages) with a EVAL-SDP-CB1Z for control through the ACE software. We are seeing SPI read/write fails using these eval kits together. The boards will work for a few minutes and then get latched up. It occurs on both LFSP and WLCSP eval boards. When the boards are working, we set the span selection to… (Show more)
in Precision DACs
dougcl
I can't believe I have to ask this here, but I can't seem to make sense of the datasheet.    On page 8 in the spec table, it says 0/AVDD (which is what I want) On page 23 it says VOUT=(2)(VREF)(x2/2^n) which gives 2.5V at x2=4095 because VREF is 1.25V     My AVDD is 3.3V. What do I need to do to get 0/3.3V out of the channels? Is it even… (Show more)
in Precision DACs
amboyle
Customer has designed in the AD5270. For production, they would like to have a way to program the devices using a PC (i.e. via USB). They have the Evaluation board for the AD5270/AD5272 devices and were wondering if it can be re-purposed to achive the goal described above.   Thanks. Anita
in Precision DACs
Maaziboy
Hi forum! I want to use HART modem AD5700-1with the intent of minimum possible complexity of operation and minimum # of components.My application is simple;i just want to make a half duplex uart bridge...i am designing a single pcb that can either take uart data in and put HART data out or take HART data in and put uart data out...the board is to… (Show more)
in Precision DACs
Load more items