Skip navigation
Log in to follow, share, and participate in this community.

Recent Activity

OliverSedlacek
The iJet MIDI-10 connection drives a JTAG debug port, so I was wondering if anyone has successfully connected to an ADuC7060 with it? It looks easy enough to wire up TMS, TCK, TDI, TDO and reset with some 100k pullups for good measure, but I'd like confirmation before I commit to copper.
in ADuC7xxx
jamesjw
Can ADuC7121 work at -40 degree C?
in ADuC7xxx
Guanhan
Hi everyone I assign the single channel PWM. But I found the PWM didn't work  when I try to config the PWM to use the P2.1. Here are the code that I assign:    int main(void) { #define GPIO_PIN1_PINFNUC_SELECT01  (0x00000010) #define GPIO_Pin1_IOState       0x020000 #define GPIO_Pin1_Outputmode    (0x02000000) #define… (Show more)
in ADuC7xxx
paulc
I bought several USB-SDP-CABLEZ Serial I/O interface for downloading FW to ADUC7020B uP.  But I cannot find either driver or SW/GUI from Analog Device website or anywhere else on the web for window 7 or window 10.    Can you please point me to right place where I can download the necessary Driver/GUI?    Thanks in advance Paul 
in ADuC7xxx
dhoni007
i am having one code where it is using look up table of various samples generating 10khz frequency but i am not getting how to generate for 1.2khz and 2.2.khz
in ADuC7xxx
Guanhan
Hi I writing to inquire Some Issues I use the ADuC 7126 QSPZ Development board to test and assign my  circuit When the Core go to the IRQ_Handler function in the  ADuC_irq.c and it goto the else loop and  always execution the while(1) loop   Function : __irq __arm void  IRQ_Handler(void) {    if ( *IRQ !=0x00)    IRQ();   else    while(1); … (Show more)
in ADuC7xxx
Penny_Xu
In what conditon, the EEPROM of ADU7023 will be modified mistakenly?Meanwhile ,watchdog reset happens. I am sure that it's not a manmade mistake. It happened occationally. I know the power supply noise could be a factor  , besides that, any other causes may lead this issue? I use the internal crystal. Our many customers complain about it.
in ADuC7xxx
Kou
Dear Sir/Madam, Is there the endurance of PLA programming of ADuC70xx? . We want to rewrite  PLA during operation. Thank you. Sincerely yours, Kou
in ADuC7xxx
jhshin
Hi all, My customer encounted an abnormal GPIO input state on ADuC7023 under specific conditions. The customer used P0.1(Pin#22) of ADuC7023 as 'GPIO input' and 0x8ea00 to 0x8f5ff of internal flash memory as the user data area. The customer also used BM = 1 and 0x80014=default value at power on reset and set the GPIO input register of P0.1 by… (Show more)
in ADuC7xxx
AndyG
I'm using the DDS function of the DAC. I've tested the DAC in normal mode, where I set values using DACDAT and get the same output range is mentioned in another post on here, however when I switch to DDS mode, I get a clean, stable sine wave, but it only uses approx. 3/4 of the full DAC output range. I can't find a specification for the DDS output… (Show more)
in ADuC7xxx
Load more items