Post Go back to editing

Synchronous signal transmission

Thread Summary

The user is experiencing issues with the synchronization signal not being mapped correctly from ports 2 and 3 of the MAX96712 to the MAX96717, resulting in high-level pins. The final answer suggests that the camera should normally be connected to a serializer, not a deserializer, and the 0x2D3 register of the MAX96717 reads 0xC, indicating a potential configuration issue.
AI Generated Content
Category: Hardware
Product Number: max96712, max967

I'm using max96712 and max96717.   When the camera is connected to ports 0 and 1 of the max96712, the synchronization signal can be normally mapped to the pins of the max96717 through the pins of the max96712.   However, when the camera is connected to port 2 and 3, after configuration mapping, the pins of the max96717 remain at a high position.   The register configuration is as follows:
96712:
0 x32c   0x83
0 x364   0x27
96717:
0 x2d5   0x87
0 x2d3   0x4
At this point, when reading the 0x2d3 register of 96717, the value is always 0xc.

Parents Reply Children
No Data