Post Go back to editing

Synchronous signal transmission

Thread Summary

The user is experiencing issues with the synchronization signal not being mapped correctly from ports 2 and 3 of the MAX96712 to the MAX96717, resulting in high-level pins. The final answer suggests that the camera should normally be connected to a serializer, not a deserializer, and the 0x2D3 register of the MAX96717 reads 0xC, indicating a potential configuration issue.
AI Generated Content
Category: Hardware
Product Number: max96712, max967

I'm using max96712 and max96717.   When the camera is connected to ports 0 and 1 of the max96712, the synchronization signal can be normally mapped to the pins of the max96717 through the pins of the max96712.   However, when the camera is connected to port 2 and 3, after configuration mapping, the pins of the max96717 remain at a high position.   The register configuration is as follows:
96712:
0 x32c   0x83
0 x364   0x27
96717:
0 x2d5   0x87
0 x2d3   0x4
At this point, when reading the 0x2d3 register of 96717, the value is always 0xc.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.