MAX9247ECM+
问答
discussion
成员
标记
Cancel
Thread Details
State
Verified Answer
Replies
3 replies
Answers
1 answer
Subscribers
2 subscribers
Views
86 views
Users
0 members are here
Options
Share
More
Cancel
Related
Post
Go back to editing
MAX9247ECM+
tonyace
on Nov 3, 2025
Thread Summary
用户询问关于MAX9247ECM+ LVDS芯片的解串器芯片信号问题。最终答案确认MAX9218的工作频率范围为7~35MHz,30MHz是可行的,但未提及是否为极限值或可能的工作稳定性问题。伴随答案建议使用MAX9248/MAX9250作为解串器。
AI Generated Content
Category:
Hardware
Product Number:
MAX9247ECM+, MAX924
您好 专家 我想使用MAX9247ECM+这个LVDS芯片,想了解一下他对应的解串器芯片的信号,希望能够得到帮助,谢谢!
MAX924
hardware
Comparators with Integrated Reference
MAX9247ECM+
comparators