Post Go back to editing

GMSL切换开关咨询

Thread Summary

The user encountered issues with camera recognition and register configuration when attempting to use the HMC544AETR switch to toggle between two 2MP cameras on a single GMSL interface with the MAX96712 deserializer. The final answer suggests that GMSL supports multiple serializers (cameras) per deserializer and recommends referring to the User Guide for detailed configuration.
AI Generated Content
Category: Hardware
Product Number: MAX96712, MAX967

您好!

   我们使用了接串器MAX96712,在单GMSL接口处,想要使用一个开关来切换两个2MP相机,尝试使用HMC544AETR芯片,出现如下问题:

1、无法识别到相机

2、识别到相机,但是配置寄存器异常

所以想要咨询下,是否有专用的GMSL接口的切换芯片?如有,请提供型号,谢谢!