Post Go back to editing

请教,AD584SH、AD584TH,在-5℃以下带载能力骤降,附原理图

AD584SH(标称4.5~30V输入,标称输出电流10mA),如图,5V输入,配置2.5V输出。

负载阻抗在350欧姆左右,2.5V/350Ω=7.14mA,AD584SH输出能力10mA,温度0℃以上,工作正常,输出2.495V;温度-5℃以下,上电后输出1.62V,工作一段时间后,输出正常2.495V(推测是工作一段时间后发热使得温度升高)。

热风枪吹,也会恢复正常2.5V。

把芯片输出更换为对地200Ω的电阻,以排除负载阻抗随温度变化,低温时输出1.25V,热风枪吹,恢复到2.5V。

更换为对地2kΩ的电阻,低温时输出2.5V。推测低温时输出能力骤降。

更换为AD584TH,与以上现象完全相同。推测排除器件批次问题。

把输入电压从5V改为12V,低温下正常输出2.5V。

请问这个现象的机制是什么,我的原理图设计有没有问题?

Parents Reply Children
  • 温度不知道。

    输入电压即电源,参考AD8029数据手册,“The output devices Q10  and Q11 work in a common-emitter configuration, and are Miller-compensated by internal capacitors, CMT  and CMB . The output voltage compliance is set by the output devices’ collector resistance RC (about 25 Ω), and by the required load current IL . ”简单讲,负载电流越大,落在Q10上的压降会越大,此时如果增加电源电压,负载电流可以继续增大。