Post Go back to editing

ltm4653 schematic

 https://www.analog.com/media/en/technical-documentation/data-sheets/ltm4653.pdf

中文:箭头所指不有两个误差放大器么(我想应该是)?正常工作时VINREG=INTVCC>2V, IMONA<2V,那么这两个误差放大器就会产生相反的输出,那么不就没有调节的作用了么?

另外为什么误差放大器要用梯形加两个圈表示?有没有相关资料证明是这样表示的,网上很难搜到这个图形。

english:there are two error amplifiers in the pic (i guess so ), when the regulator works in normal mode,VINREG=INTVCC>2V, IMONA<2V,then the output of the two erroe amplifiers are different ,so can the error amplifiers achieve its functiona described in the datasheets?