Post Go back to editing

TMC9660-3PH-BL 开发板Could not identify the connected chip

Thread Summary

The user encountered an error 'Could not identify the connected chip' when using the TMC9660-3PH-BL development board, due to an unsupported Landungsbruecke firmware version. The solution is to update the Landungsbruecke firmware to version 3.11.4 using the IDE's download function. The provided firmware file is LandungsbrueckeV3_v3.11.4_BL.hex.zip.
AI Generated Content

hi 专家您好,

我使用TMC9660-3PH-BL 开发板点击Inspect chip后显示:Error: Could not identify the connected chip. Ensure that the communication is functional.

This error occurs when the GET_INFO command for the chip type does not return the expected value of 0x544D0001.

查看打印显示:Selection is not supported! ID33: TMC9660-3PH-EVAL (BOOT) is not supported by Landungsbruecke firmware [V 3.09.1];请问如何处理才能扫到片上chip;目前IDE使用4.9.0最新版本

Parents Reply Children
No Data